This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

float licence issue tidspssw exited with status 45


Linux VB 3.13.0-53-generic #89-Ubuntu SMP Wed May 20 10:34:39 UTC 2015 x86_64 x86_64 x86_64 GNU/Linux # root at VB in /opt/license_server [12:21:35] $ tree . ├── bin │ ├── lmdiag │ ├── lmgrd │ ├── lmutil │ └── tidspssw ├── licenses │ └── TMDSCCS-ALLF01-v6.lic └── logs └── tidspssw.log 3 directories, 6 files # longqi at VB in /opt/license_server [12:24:17] $ /opt/license_server/bin/lmgrd -c /opt/license_server/licenses/TMDSCCS-ALLF01-v6.lic 12:24:21 (lmgrd) ----------------------------------------------- 12:24:21 (lmgrd) Please Note: 12:24:21 (lmgrd) 12:24:21 (lmgrd) This log is intended for debug purposes only. 12:24:21 (lmgrd) In order to capture accurate license 12:24:21 (lmgrd) usage data into an organized repository, 12:24:21 (lmgrd) please enable report logging. Use Flexera Software LLC's 12:24:21 (lmgrd) software license administration solution, 12:24:21 (lmgrd) FlexNet Manager, to readily gain visibility 12:24:21 (lmgrd) into license usage data and to create 12:24:21 (lmgrd) insightful reports on critical information like 12:24:21 (lmgrd) license availability and usage. FlexNet Manager 12:24:21 (lmgrd) can be fully automated to run these reports on 12:24:21 (lmgrd) schedule and can be used to track license 12:24:21 (lmgrd) servers and usage across a heterogeneous 12:24:21 (lmgrd) network of servers including Windows NT, Linux 12:24:21 (lmgrd) and UNIX. Contact Flexera Software LLC at 12:24:21 (lmgrd) www.flexerasoftware.com for more details on how to 12:24:21 (lmgrd) obtain an evaluation copy of FlexNet Manager 12:24:21 (lmgrd) for your enterprise. 12:24:21 (lmgrd) 12:24:21 (lmgrd) ----------------------------------------------- 12:24:21 (lmgrd) 12:24:21 (lmgrd) 12:24:21 (lmgrd) Server's System Date and Time: Wed Jun 03 2015 12:24:21 SGT 12:24:21 (lmgrd) SLOG: Summary LOG statistics is enabled. 12:24:21 (lmgrd) Can't make directory /usr/tmp/.flexlm, errno: 2(No such file or directory) 12:24:21 (lmgrd) FlexNet Licensing (v11.12.1.1 build 150159 i86_lsb) started on VB (linux) (6/3/2015) 12:24:21 (lmgrd) Copyright (c) 1988-2014 Flexera Software LLC. All Rights Reserved. 12:24:21 (lmgrd) World Wide Web: http://www.flexerasoftware.com 12:24:21 (lmgrd) License file(s): /opt/license_server/licenses/TMDSCCS-ALLF01-v6.lic 12:24:21 (lmgrd) lmgrd tcp-port 27000 12:24:21 (lmgrd) (@lmgrd-SLOG@) =============================================== 12:24:21 (lmgrd) (@lmgrd-SLOG@) === LMGRD === 12:24:21 (lmgrd) (@lmgrd-SLOG@) Start-Date: Wed Jun 03 2015 12:24:21 SGT 12:24:21 (lmgrd) (@lmgrd-SLOG@) PID: 3961 12:24:21 (lmgrd) (@lmgrd-SLOG@) LMGRD Version: v11.12.1.1 build 150159 i86_lsb ( build 150159 (ipv6)) 12:24:21 (lmgrd) (@lmgrd-SLOG@) 12:24:21 (lmgrd) (@lmgrd-SLOG@) === Network Info === 12:24:21 (lmgrd) (@lmgrd-SLOG@) Socket interface: IPV6 12:24:21 (lmgrd) (@lmgrd-SLOG@) Listening port: 27000 12:24:21 (lmgrd) (@lmgrd-SLOG@) 12:24:21 (lmgrd) (@lmgrd-SLOG@) === Startup Info === 12:24:21 (lmgrd) (@lmgrd-SLOG@) Server Configuration: Single Server 12:24:21 (lmgrd) (@lmgrd-SLOG@) Command-line options used at LS startup: -c /opt/license_server/licenses/TMDSCCS-ALLF01-v6.lic 12:24:21 (lmgrd) (@lmgrd-SLOG@) License file(s) used: /opt/license_server/licenses/TMDSCCS-ALLF01-v6.lic 12:24:21 (lmgrd) (@lmgrd-SLOG@) =============================================== 12:24:21 (lmgrd) Starting vendor daemons ... 12:24:21 (lmgrd) Started tidspssw (internet tcp_port 41700 pid 3966) 12:24:21 (lmgrd) license daemon: execute process failed: (/opt/license_server/bin/tidspssw) -T VB 11.12 3 -c /opt/license_server/licenses/TMDSCCS-ALLF01-v6.lic 12:24:21 (lmgrd) license daemon: system error code: No such file or directory 12:24:21 (lmgrd) tidspssw exited with status 45 (Child cannot exec requested server) 12:24:21 (lmgrd) Please correct problem and restart daemons

  • Hi,

    A number of issues may cause such error, including invalid path (which looks fine by me) or file access permissions to the tidspssw (directory and file read permissions for regular users, for example). Can you double check these details?

    Hope this helps,
    Rafael
  • The permission is OK. You can see this:

    # longqi at VB in /opt/license_server [18:55:57]
    $ ll bin licenses logs 
    bin:
    total 3.3M
    -rwxrwxrwx 1 longqi longqi 1006K Nov  7  2014 lmdiag
    -rwxrwxrwx 1 longqi longqi  1.1M Nov  7  2014 lmgrd
    -rwxrwxrwx 1 longqi longqi 1006K Nov  7  2014 lmutil
    -rwxrwxrwx 1 longqi longqi  165K Jun  3 10:38 tidspssw
    
    licenses:
    total 4.0K
    -rwxrwxrwx 1 longqi longqi 1.2K Jun  3 10:39 TMDSCCS-ALLF01-v6.lic
    
    logs:
    total 4.0K
    -rwxrwxrwx 1 longqi longqi    0 Aug 13 18:40 boot.log
    -rw-rw-r-- 1 longqi longqi 3.4K Aug 13 18:55 tidspssw.log
    

  • The Linux I'm using is VirtualBox. Is it the reason?