Other Parts Discussed in Thread: ENERGIA
I'm using CCS6.01 for MSP430 and can compile then debug OK.
The problem is that I CANNOT SEE THE "RUN" options : Resume. Suspend. Terminate. Step-into. ETCETERA
This is either on the Icon line OR in the drop-down 'Run' tab.
All of them are faded out, so cannot be selected.
When I first started using CCS6 a few days ago, running Blink example, these options were visible & selectable.
Now they are not there !!
How can I re-enable these essential selections ???