Hi,
I have Code Composer Studio 5.5.0.00077 and when I add a new driver files to my project (.h and .c) and try to save as I make changes I get an error.
Windows Vista Service Pack 1
I added them in Code Composer (File->New-> Source File, and File->New->Header File). Also tried select and drag from Windows file explorer to Code Composer Studio project.
"C/C++ Indexer has encountered a problem.
An internal error occurred during: "C/C++ Indexer".
Looking at the Error Log I see:
1. An internal error occurred during: "C/C++ Indexer".
2. Error in CDT Core during AST creation
3. Problems occurred when invoking code from plug-in: "org.eclipse.cdt.core".
Only the new files cause these errors in the Error Log. The original files in this project do not.
In Code Composer I just click in the file and I get these Errors (2, 3).
Any help is appreciated.
Regards,
Ed