I got a XDS560v2 from other team for which USB is not working. Not sure whats the problem with USB, but Ethernet is working.
It has static IP assigned to it, which is outside our LAN network.
Used a Ethernet switch (hub) and configured static IP (in same series as of JTAG ) to my Laptop and connected both Laptop and JTAG to Switch.
I could able to ping the JTAG and use it via CCS. ( SDconfig utility is not detecting JTAG, but CCSv5 detects fine)
I would like to change the IP address for the JTAG to put it in to our LAN.
Is there anyway to change IP address for the JTAG (when USB is not working). Or is it possible to change it to Dynamic IP.