This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problems with the compiler version

Hi there!

I'm having problems with the compiler version. I changed my PC, and instaled the last version (CCS6.1). Now I have a warning: 

Description Resource Path Location Type
This project was created using a version of compiler that is not currently installed: 4.3.1 [MSP430]. Another version of the compiler will be used during build: 4.4.5. Please go to <a href="liveaction:OpenAppCenter">CCS App Center</a> to install the compiler of the required version, or migrate the project to one of the available compiler versions by adjusting project properties. EPS_MAIN_PROG_TRIAL_V1 properties Problems

Migrate the project has any disadvantage?