This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Code size limit exceeded on MSP430F5638, 4K limit w/ full license?!?!?!?!

Reinstalled CCS6.  Received license from TI.  Chip has 256K FLASH.

Apparently CCS doesn't think so, it seems to have retained its 4K limit:

Typical message 
 "./lnk.cmd", line 48: error #10099-D: program will not fit into available
    memory.  placement with alignment fails for section ".text" size 0x2b12 .
    Available memory ranges:
    FLASH        size: 0x1000       unused: 0xe56        max hole: 0xe56    


What it means 

The linker was unable to fit some portion of the program onto the device. The specific error message indicates what section of the program the linker failed to place, its size, and the memory range it tried to place it in. For the memory ranges listed, the size indicates the total size of the section, unused represents the amount of space remaining when trying to place the section that failed and max hole represents the largest contiguous region available.

Why is it happening 

Fundamentally, this indicates that the device has insufficient physical memory (read-only or read-write) to handle the program. However, this doesn't necessarily mean that a larger device is required. There are several things that can be changed that could resolve the problem. Also, for advanced users this error could also come from an incorrect linker command file that doesn't accurately represent the current device. (TI devices normally come with an appropriate linker command file and don't require user modification, so if you don't know anything about the linker command file you shouldn't worry about this possibility.)

Remedy 

This error message can occur for several reasons so there are multiple possible solutions. A few common issues to consider: 
• If a section failed to place to RAM make sure that the stack and heap sizes are set appropriately for the device and your program. Consider reducing them. 
• Try enabling or increasing the optimization level used by the compiler. Unoptimized programs require far more space than optimized ones. 
• If you have added I/O code for debugging purposes this can be larger than expected. Specifically, printf() will not fit on many small embedded devices. Depending on the size of the device, the --printf_support=minimal option may solve the problem or printf() may not be a viable means of debugging at all. 


If the above suggestions don't resolve the issue then more investigation will be required to determine if the issue is simply that the device is not large enough for the program or if space is being used unnecessarily. The best place to find more information is the map file generated by the linker. The map file provides detailed information on where sections are placed, what they consist of and how large they are. When looking at this please keep in mind that the section that failed to place is not necessarily the source of the problem. Another section previously placed in the same memory region could have been much larger than expected and introduced the issue.

Risks, Severity 

This error prevents the construction of an executable program.

Anyone have any idea why a fully licensed CCS would be pulling this on me?

Ed Averill