Hi ,
im using a OMAP l138 LCDK , XDS100v2 debugger and CCS 6.x . If i want to connect to the Arm core i get this message :ARM9_0: Output: Target Connected.
ARM9_0: Output: ---------------------------------------------
ARM9_0: Output: Memory Map Cleared.
ARM9_0: Output: ---------------------------------------------
ARM9_0: Output: Memory Map Setup Complete.
ARM9_0: Output: ---------------------------------------------
ARM9_0: Output: KICK Unlocked.
ARM9_0: Output: ---------------------------------------------
ARM9_0: Output: PSC Enable Complete.
ARM9_0: Output: ---------------------------------------------
ARM9_0: GEL: Error while executing OnTargetConnect(): Target failed to write 0x01C11138
at (*((unsigned int *) (0x01C11000+0x138))|=0x1) [OMAPL138_ARM.gel:16]
at device_PLL0(0, 24, 1, 0, 1, 11, 5) [OMAPL138_ARM.gel:400]
at Set_Core_300MHz() [OMAPL138_ARM.gel:459]
at Core_300MHz_mDDR_150MHz() [OMAPL138_ARM.gel:247]
at OnTargetConnect()
The problem itself is not new , but the anser that helps everyone else( changing the TCLK to adaptive) is not working for me , because i get this message:
Error connecting to the target:
(Error -150 @ 0x0)
One of the FTDI driver functions used during
configuration returned a invalid status or an error.
(Emulation package 5.1.641.0)
i have changed the gel files(from your site and pd's), took the step rate down to very slow and updated the xds100v2 firmware .
I got no idea.
Best Regards