Hi I have an issue The task sleep and timer interrupt is not working with the simulator setup. I have gone through the following link and tired the changes mentioned in this but still I was not sucessfull. the Swi post is working but task sleep and timer is not working.
http://processors.wiki.ti.com/index.php/C64x%2B_CPU_Cycle_Accurate_Simulator
Following version I use:
BIOS version:6.34.4.22
XDC version :3.24.5.48
compiler:Tiv.7.4.4
ti.platforms.sim64Pxx
ti.targets.C64P
Code Composer Studio Version: 5.5.0.00077