This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am experiencing a problem where I cannot read the value of a pointer and display it in a textbox.
Following the example given here http://processors.wiki.ti.com/index.php/GUI_Composer/Bind_Expressions I am not able to display anything.
I tried both using array variables of an object, global array variable or simple int* variable. The result was the same: nothing gets displayed in the textBox. This is the related content of app.json:
"serverBindName": "evaluate['*(ObjectInstance.UDC[0])']", // As done in CCS Debug view (shows the correct value) or "serverBindName": "evaluate['*UDCvalueptr[0]']", or "serverBindName": "evaluate['*UDCvalueptr_moduleA']",
For reference the following works correctly:
"serverBindName": "ObjectInstance.VariableNotPointer[0]",
I'm using GUI composer runtime 5.5.0.2 runtime with Code Composer Studio 5.5.0.00077. Target is TMS320C28346 using JTAG Spectrum Digital XDS510 USB.
Since this project is managed in a team upgrading to CCS v6/v6.1 is not an option unfortutanely.
Any help would be greatly appreciated. Thank you in advance to all of you!
Sorry Stefano, the above link to Bind expressions wiki page is the only reference link. Let me call in Patrick Chuong to guide you.
Goodluck & Regards,
Gautam