This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS5.2.1.00018 can't create project for 6678

I want to create a project for 6678 in CCS 5.2,

in the pop-up dialog, I chose the following options:

Family->6000

Variant->C66xx Multicore DSP, but in the right list  only TMS320C6657 is selectable

Please help!

thanks!

  • Hello,
    Earlier versions of CCS was missing some specific device support integration with the Project Wizard. You can use "Generic devices -> Generic C66xx Device" in your case. That is the option used by C6678 customers on CCSv5.2.

    Or, you can also choose to update your CCS version. CCSv5.5 has this integration.

    Thanks
    ki