Other Parts Discussed in Thread: MSP430AFE252, MSP430F6736
Hello ,
I have to convert my existing IAR code into CCS v6
I have tried it but facing some issue ,tried to solve it, seen lots of forums ,but cant able to solve it
please see the compiler console below of my code ,so can some one help me ,how to resolve this problem.
i am working on Energy meter project.
**** Build of configuration Debug for project AV_BI_AFE252_Rev1.1 ****
C:\ti\ccsv5\utils\bin\gmake -k all
'Building target: AV_BI_AFE252_Rev1.1.out'
'Invoking: MSP430 Linker'
"C:/ti/ccsv5/tools/compiler/msp430/bin/cl430" -vmsp --abi=coffabi -g --define=__MSP430AFE252__ --diag_warning=225 --display_error_number --printf_support=minimal -z -m"AV_BI_AFE252_Rev1.1.map" --stack_size=80 --heap_size=80 --use_hw_mpy=16 -i"C:/ti/ccsv5/ccs_base/msp430/include" -i"C:/ti/ccsv5/tools/compiler/msp430/lib" -i"C:/ti/ccsv5/tools/compiler/msp430/include" --reread_libs --warn_sections --rom_model -o "AV_BI_AFE252_Rev1.1.out" "./source/Tamper_Storage.obj" "./source/RTC_RD_WR.obj" "./source/IR_Communication.obj" "./source/Emeter_RTC.obj" "./source/Emeter_Main.obj" "./source/Emeter_LPM.obj" "./source/Emeter_Key_Init.obj" "./source/Emeter_KWh_MD.obj" "./source/Emeter_Interrupts.obj" "./source/Emeter_Init.obj" "./source/Emeter_I2C.obj" "./source/Emeter_Functions.obj" "./source/Emeter_Eeprom_RW.obj" "./source/Emeter_Calib.obj" "./source/Emeter_Calculation.obj" -l"libc.a" "../lnk_msp430afe252.cmd"
<Linking>
undefined first referenced
symbol in file
--------- ----------------
_P1DIR ./source/Emeter_Init.obj
_P1OUT ./source/Emeter_Main.obj
_P2DIR ./source/Emeter_Init.obj
_P2OUT ./source/Emeter_Init.obj
error #10234-D: unresolved symbols remain
error #10010: errors encountered during linking; "AV_BI_AFE252_Rev1.1.out" not
built
>> Compilation failure
gmake: *** [AV_BI_AFE252_Rev1.1.out] Error 1
gmake: Target `all' not remade because of errors.
**** Build Finished ****