Other Parts Discussed in Thread: OMAP-L138, OMAPL138
Hi,
Here is my configuration:
- CCS v5.5,
- OMAP-L138 (Avanet Spartan-6/OMAP-L138 Co-Processing Development Kit),
- Blackhawk XDS560v2-USB,
- SYS/BIOS 6.35.4.50.
I created the project Example Log from the example project (SYS/BIOS->C6000->OMAP-L1x->EVMOMAPL138->Generic examples->Log Example). I used the default OMAPL138.ccxml. I builded the project without errors and I clicked Debug. Balckhawk emulator is ok. I tested it with file OMAPL138.ccxml -> Test connection. It passed it.
The problem is that in Debug mode program is still running. It should be stopped by CCS on the beginning. When I use SYS/BIOS its continuously running. When I don't use SYS/BIOS (program has been written in C), after Debug program is suspended and then I can debug it line by line:
When I'm using SYS/BIOS program is running. Even when I put breakpoint in a code and then run debug mode, program ist still running.
How can I configure CCS v5.5 in order to use the debug mode and SYS/BIOS? Is there any option, that should I mark? I'd like to have situation that program is stopping on the beginning.
Thank you.