This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

code composer studio on windows 10



Im running CCS 6 on windows 10 and everything is really small. For instance when it starts the splash screen appears as normal but after a second or so it shrinks to the size of a thumbnail in the top right of the screen. After it starts all of the buttons are too small to see. None of the windows settings regarding size and resolution seem to fix this. Is this a known issue?