Other Parts Discussed in Thread: UNIFLASH, CC2650
Hi There,
I have an XDS200 USB which works fine on windows with CCS but can't be detected on Uniflash 3.4 on Ubuntu 14.04 64 bit.
I have no problem getting a XDS100V3 on a SmartRF06 to connect on Uniflash on the same USB port with the same USB cable but the XDS200 just can't get connected.
The error messages in Uniflash are
[18:11:49] ERROR >> IcePick_C: Error initializing emulator: (Error -2083 @ 0x0) Unable to communicate with the debug probe. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation. (Emulation package 6.0.14.5)
[18:11:51] com.ti.debug.engine.IApplication$InitializationException: IcePick_C: Error initializing emulator: (Error -2083 @ 0x0) Unable to communicate with the debug probe. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation. (Emulation package 6.0.14.5)
Running lsusb shows up the device and when I unplug it, the entry goes away.
Bus 002 Device 010: ID 0451:bef0 Texas Instruments, Inc.
Likewise the following entries are there on etc/ttyACMn entries when the XDS200 is plugged in and not there when it is unplugged
$ dir ttyAC*
ttyACM0 ttyACM1
I have tried plugging the device into different USB ports on the mobile workstation and restarting Uniflash but nothing seems to work.
I am trying to connect to a cc2650 processor. I did this with no issues with the WDS100V3 on this linux machine and I have done the same with the XDS200 on a windows machine but the XDS200 does not seem to work on Linux.
I have updated the Uniflash 3.4 with the latest updates.
What am I missing and how do I move forward?
Thanks for any help!
cheers
Peter