We have had working environments for flashing and debugging our TMS320LF2406A PCBA. This is an old product for us, so JTAG is seldom used, but it is essential when we get problems and need to analyse them. We are now facing a potentially hugh Q-issue and really need to get a debugger up and running to view the contents of the internal memories.
Our SW engineers have typically helped out when issues arise, but they have all moved on to Win 7 and can no longer offer assistance so I have tried to set up an environment on two different older computers that still run Win XP.
I have managed to install SD drivers for the XDS510 USB, and their diagnsostic tool says everything is fine, but I cannot get CCS 3.3 to connect to the target via the XDS510. CCS4.xx onwards does not support 240x devices so I cannot update ... .
Error dialog fron CCS 3.3 says:
Error initializing emulator
I/O Port = 510
Board Name: F2406A XDS510USB Emulator
Cpu Name: cpu_0
SD diagnostic says:
** Checking emulator/eZdsp scan connection
** Emulator Test **
$$ EmuProductName=XDS510USB
$$ EmuPortAddr=0x510
$$ EmuPortMode=USB
$$ ProductId=510
$$ ProductVersion=84
** Emulator Scan Test
-- Found JTAG IR length of 8
-- Found 1 JTAG device(s) in the scan chain