This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Unresolved symbols using static library in CCS6



I've recently started working with a Tiva C dev board and CCS6. I'm trying to create a library to use from different projects. I've taken the following steps:

  1. I've created a new CCS project and designated it as a Static Library.
  2. In the project that I wish to reference my library files from, I add the library project to the include path for both the ARM Compiler and ARM Linker.
  3. I then #include the appropriate headers but when I build, all functions defined in the libraries generate unsolved symbol errors.

What critical piece am I missing? I'm using other includes from the Tivaware libs using a variable path definition with no problems.

Any suggestions would be greatly appreciated.