This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAP L138 connecting problem with CCS 4.1.2

Other Parts Discussed in Thread: OMAPL138

 

hi

i have downloaded new CCS 4.1.2, i am trying to connect to OMAP L138 with the help of XDS100V2(vista OS)

 

when i do a connect

nothing happens, not even my gel script gets executed

 

ravindra

 

  • Ravindra,

    Does CCS try to connect?  Does your device status change to "Connected" or does it stall trying to connect?  Do you get any error messages?  Have you updated your XDS100v2 ( http://processors.wiki.ti.com/index.php/XDS100#Q:_How_can_I_update_the_CPLD_on_my_XDS100v2.3F )?

    -Tommy

  • I had a similar experience with my Stellaris Dev. kits. I had CCS 4.1.1 loaded, and when CCS came up, it asked me if I wanted to upgrade. I checked what it wanted to upgrade:

    • 4.1.2.00027  Service Release
    • MSP430 Code Generation Tools 3.2.3
    • TMS470 Code Generation Tools 4.6.3

    When I let CCS upgrade itself, all communications to my Dev. Kit boards ceased. Same symptoms.

    I uninstalled CCS 4.1.2 and re-installed 4.1.1, and everything started working again.

  • My experience was that CCS stalled in trying to connect to target, and it never timed out. I closed CCS to resolve the stalling issue.

    No error messages.

  •  

    hi tommy

    i did not get any error messages (i will get back to you on the status)

    1) about the cpld update ,,,, is it safe to do that, because i guess the changes cannot be reverted back(is it backward compatable)

    2) do you have any updates about the problems in CCS4.1.2 with omp l138(or should i download 4.1.1)

    3) perviously i was using CCS4.0.xxx, in that i wgen i selected xds100V2 i did not get target named omap l138,,,, instead i use to connect using L137,,,,, can you help me in    solving this

    4) one more thing i wanted to say was, that the board is loaded with linux ,,,,, and i am trying to connect to it while its booting is this  a problem

     

    ravindra

     

     

  • ravindra mudreddy said:
    1) about the cpld update ,,,, is it safe to do that, because i guess the changes cannot be reverted back(is it backward compatable)

    Yes, the CPLD has been checked out by a number of internal users and has proven to be safe thus far.

    ravindra mudreddy said:
    2) do you have any updates about the problems in CCS4.1.2 with omp l138(or should i download 4.1.1)

    I am not aware of any problems specific to CCS4.1.2.

    ravindra mudreddy said:
    3) perviously i was using CCS4.0.xxx, in that i wgen i selected xds100V2 i did not get target named omap l138,,,, instead i use to connect using L137,,,,, can you help me in    solving this

    I think this was an honest mistake.  XDS100v2 is supported for OMAPL138 and the hardware setup is compatible between the two devices.

    ravindra mudreddy said:
    4) one more thing i wanted to say was, that the board is loaded with linux ,,,,, and i am trying to connect to it while its booting is this  a problem

    There may be some issues to work around when connecting to ARM actively running Linux vs plain C-code.  The CCS team recently completed this article for Linux-aware debug with CCS4: http://processors.wiki.ti.com/index.php/Linux_Aware_Debug

  • I'd like to chime in on this problem since I'm seeing a similar problem. I'm also running CCS 4.1.2 (on Windows XP) and I'm using the XDS100V2 to connect to the Omap L138 eXperimenters kit, and I get the following error message in CCS4:

    "Arm9_0:gel:error while executing OnTargetConnect():attempted to read unmapped virtual memory at 0X01C10800:failed to get PRSC status.

    This gel file works with the eXperimenters kit when I use the XDS510 USB emulator instead of the XDS100v2. (It's the gel file that is supplied by Logic PD for the eXperimenters kit.) This memory location is a PRSC status register, so why would it look like unmapped virtual memory?

    Thanks,

    JV

  • hi JV

    i had also the same error , what i did was

     

    As soon as power up the board i quickly luanch "debug active project" as soon as i can, because linux starts booting on my board this helped me  solveing the error

    if i do manual "connect" and "load program" i still the error you mentioned

    you can try it out

    Jv,Tommy

    Now i getting error

    "ARM9_0: Loader: One or more sections of your program falls into a memory region that is not writable. These regions will not actually be written to the target. Check your linker configuration and/or memory map."

    i am using the following linker config

    -l ..\evmomapl138_bsl.lib

    -stack           0x00000800
    -heap            0x00000800

    MEMORY
    {
       dsp_l2_ram:      ORIGIN = 0x11800000  LENGTH = 0x00040000
       shared_ram:      ORIGIN = 0x80000000  LENGTH = 0x00020000
       external_ram:    ORIGIN = 0xC0000000  LENGTH = 0x08000000
       arm_local_ram:   ORIGIN = 0xFFFF0000  LENGTH = 0x00002000
    }

    SECTIONS
    {
       .text       > shared_ram
       .const      > shared_ram
       .bss        > shared_ram
       .far        > shared_ram
       .switch     > shared_ram
       .stack      > shared_ram
       .data       > shared_ram
       .cinit      > shared_ram
       .sysmem     > shared_ram
       .cio        > shared_ram
    }

     

    can you help me with this

    ravindra

  • JV,

    Have you updated your XDS100v2 CPLD?  That has fixed a number of known emulator issues.

    -Tommy

  • Ravindra,

    I would recommend that you try the emulation boot mode (Switch7[8:5] = ON-OFF-OFF-ON) if you want to load a program to ARM.  Depending on where you catch the Linux boot process, virtual memory may or may not be enabled, which would create memory-map issues.

    Are you given any hints as to which variable(s) or function(s) are falling into the invalid memory section?

    -Tommy

  • I have the same experience running CCS 4.1.2 and trying to connect to any of my Stellaris dev boards. I am running Vista 32 bits Home Premium. However, 4.1.2 runs OK under XP Pro SP3 if you remove the firewall block.

     

    Any suggstions on how to get 4.1.2 working under Vista?

  • José,

    Please check the wiki topic below:

    http://processors.wiki.ti.com/index.php/Vista_with_CCS

    I've been using CCSv4 with Vista for a while now and it works fine.

    Hope this helps,

    Rafael

  • hi

    desouza, rafael

     Are you sure with that, beacuse i dont have a ccs starting problem ,,,,,,,,,,,,,,,, i have problem in the memory section while loading

    if confirm i will reinstall CCS in a different folder

     

    tommy

    i will try to update CPLD and let you know

    and the question you asked about any hints of function or variables i am not getting any

    can you please let me know with above linker config from which address to which address code,variables etcc are  dumped , or send me the link from where i can read about this

    ravindra

     

  • I updated the XDS100V2 emulator's CPLD file, and I've tried this emulator on three different PCs with the same results. On the eXperimenters kit the emulator runs the GEL file until it tries to set the system clock to 300MHz and then it hangs up and times out. I tried setting the 'fast arm download' setting to 'off' and setting the timeout delay to 'very slow'. I get the same results on our new prototype design which has no linux code loaded. I tried changing the system clock/DDR clock settings from 300MHz/132MHz to 200MHz/126MHz but it still hangs. Should this problem be directed to Spectrum Digital or should it be handled through this forum?

  • After some more debugging I can see that the startup hang problem is not limited to the XDS100V2 emulator, because it also happens with the XDS510PP emulator as well. The XDS510USB emulator works fine. I've isolated the place in the Logic PD GEL file that hangs up. It's in this function:

    device_PLL0(unsigned int CLKMODE, unsigned int PLLM, unsigned int POSTDIV,unsigned int PLLDIV1, unsigned int PLLDIV2, unsigned int PLLDIV3, unsigned int PLLDIV7 ) {

     

    unsigned int i=0;

    /* Clear PLL lock bit */

    CFGCHIP0 &= ~(0x00000010);

     

    /* Set PLLENSRC '0',bit 5, PLL Enable(PLLEN) selection is controlled through MMR */

    PLL0_PLLCTL &= ~(0x00000020);

     

    /* PLLCTL.EXTCLKSRC bit 9 should be left at 0 for Freon */

    PLL0_PLLCTL &= ~(0x00000200);

     

    /* Set PLLEN=0 to put in bypass mode*/

    PLL0_PLLCTL &= ~(0x00000001);

     

    /*wait for 4 cycles to allow PLLEN mux switches properly to bypass clock*/

    for(i=0; i<PLLEN_MUX_SWITCH; i++) {;}

     

    /* Select the Clock Mode bit 8 as External Clock or On Chip Oscilator*/

    GEL_TextOut("\tbefore PLL0_PLLCTL read, in PLL config function.\n","Output",1,1,1);

    PLL0_PLLCTL &= 0xFFFFFEFF;

    GEL_TextOut("\tafter PLL0_PLLCTL read, in PLL config function.\n","Output",1,1,1);

    PLL0_PLLCTL |= (CLKMODE << 8);

    I added the GEL_TextOut lines at the end of this function, and the second GEL_TextOut line never executes, so the emulator hangs up waiting to read the PLL0_PLLCTL register. This is confirmed on the console printout that says the emulator was unable to read address 0x01C11100, which is the address of the PLL0_PLLCTL register. I tried increasing the 4 cycle delay in the function before the register read to 1000 cycles, but that didn't fix it.

    My guess is that these emulators have trouble communicating with the target chip when its system clock is being punched around (not too surprising). The XDS510USB emulator can survive this though, maybe because it retries JTAG communications whereas the XDS100V2 and the XDS510PP don't or something like that. If you guys at TI want me to try anything else to help fix this let me know.

    -JV

  • Adaptive clocking fixed it, thanks Tommy!

  • hi all

    i have updated the cpld on my xds100v2 ,,, and landed in big  trouble,,,, first i was not able to load my program,,,now i am not even able to connect to the target,,,, i am getting icecrusher errors

    can any body help me

    ARM9_0: Error connecting to the target: 0x80000240/-2062 @ marker 13008 Fatal Error during: Initialization, OCS, Cannot halt the processor

    ARM9_0: Warning: 0x40000240/-1029 @ marker 11103 Warning during: Initialization, OCS, The ICECrusher register scan returned invalid data

    ARM9_0: Warning: 0x40000240/-1029 @ marker 11103 Warning during: Initialization, OCS, The ICECrusher register scan returned invalid data

    ARM9_0: Warning: 0x40020244/-1029 @ marker 11103 Warning during: Register, Initialization, OCS, Internal, The ICECrusher register scan returned invalid data

    ARM9_0: Warning: 0x40000240/-1029 @ marker 11103 Warning during: Initialization, OCS, The ICECrusher register scan returned invalid data

    ARM9_0: Warning: 0x40000240/-1029 @ marker 11103 Warning during: Initialization, OCS, The ICECrusher register scan returned invalid data

    ARM9_0: Warning: 0x40000240/-1029 @ marker 11103 Warning during: Initialization, OCS, The ICECrusher register scan returned invalid data

    ARM9_0: Error connecting to the target: 0x80000240/-2062 @ marker 13008 Fatal Error during: Initialization, OCS, Cannot halt the processor

    ARM9_0: Error connecting to the target: 0x80000240/-2062 @ marker 13008 Fatal Error during: Initialization, OCS, Cannot halt the processor

    ARM9_0: Warning: 0x40000240/-1029 @ marker 11103 Warning during: Initialization, OCS, The ICECrusher register scan returned invalid data

    ARM9_0: Warning: 0x40000240/-1029 @ marker 11103 Warning during: Initialization, OCS, The ICECrusher register scan returned invalid data

    ARM9_0: Error connecting to the target: 0x80000240/-2062 @ marker 13008 Fatal Error during: Initialization, OCS, Cannot halt the processor

    ARM9_0: Warning: 0x40000240/-1029 @ marker 11103 Warning during: Initialization, OCS, The ICECrusher register scan returned invalid data

  • Ravindra,

    Did you enable adaptive clocking?

    -Tommy

  • I believe I have seen a similar issue on a different device, and JV is right.

    Without getting into all of the details. the basic solution is to program the PLL through target code, not through GEL.  This problem is limited to ARM processors, as far as I know.  Two sources of the problem are mentioned below.

    1)       Programming the PLL from GEL is historically problematic as the core clock will cause RTCK to modulate and TCK may not be slow enough.

    2)       The TI on-chip adaptive clock support appears to have some issues if TCK is stopped/restarted.  When doing TCK clock stop operation we normally turn off TI on-chip adaptive clocking and let the emulator do the right thing. The XDS100V2 is supposed to have this feature but I do not think it was ever enabled in USCIF for XDS100v2.

     

  • yes i did turn on adaptive clocking

  • danr

    so what are my options now

    if i do simple connecte with out gel file(linux is already booting in the background) , i am getting the same errors

    ravindra

  • The only validated option is to boot code that initializes the PLL rather than trying to have GEL do it for you.

     

     

     

  • tlee said:
    I would recommend that you try the emulation boot mode (Switch7[8:5] = ON-OFF-OFF-ON) if you want to load a program to ARM.  Depending on where you catch the Linux boot process, virtual memory may or may not be enabled, which would create memory-map issues.

    Did you ever try this suggestion from Tommy?  I think using "emulation boot" plus "adaptive clocking" is key.  

  •  

    hi brad

    i tried with it but the errors are same

     i am getting the following errors only , only after i updated my CPLD in XDS100v2

    ARM9_0: Error connecting to the target: 0x80000240/-2062 @ marker 13008 Fatal Error during: Initialization, OCS, Cannot halt the processor

    ARM9_0: Warning: 0x40020244/-1029 @ marker 11103 Warning during: Register, Initialization, OCS, Internal, The ICECrusher register scan returned invalid data

    ARM9_0: Warning: 0x40000240/-1029 @ marker 11103 Warning during: Initialization, OCS, The ICECrusher register scan returned invalid data

    ARM9_0: Warning: 0x40000240/-1029 @ marker 11103 Warning during: Initialization, OCS, The ICECrusher register scan returned invalid data

    ARM9_0: Warning: 0x40000240/-1029 @ marker 11103 Warning during: Initialization, OCS, The ICECrusher register scan returned invalid data

    ARM9_0: Warning: 0x40000240/-1029 @ marker 11103 Warning during: Initialization, OCS, The ICECrusher register scan returned invalid data

    ARM9_0: Warning: 0x40000240/-1029 @ marker 11103 Warning during: Initialization, OCS, The ICECrusher register scan returned invalid data

    ARM9_0: Warning: 0x40000240/-1029 @ marker 11103 Warning during: Initialization, OCS, The ICECrusher register scan returned invalid data

    ARM9_0: Error connecting to the target: 0x80000240/-2062 @ marker 13008 Fatal Error during: Initialization, OCS, Cannot halt the processor

    ARM9_0: Warning: 0x40020204/-1026 @ marker 11112 Warning during: Register, OCS, Internal, The resource has not been claimed

     

     

     

    after i do the multiple "retry" "retry",,,,,,device is shown as connected in CCS

    but when i load the program i get the below error and my program is loaded

    "

    ARM9_0: File Loader: Data verification failed at address 0x80000000 Please verify target memory and memory map.

    ARM9_0: Unable to terminate memory download: 0x00000004/-2030 @ marker 583696133 Error during: Register, Access to an unknown or invalid register was attempted.

    Error found during data verification.

    Ensure the linker command file matches the memory map."

     

    1) can you please help me with this,,,

    2) is there any way that i role back my CPLD version to the orignal thing

    thanks & regards

    ravindra

  • Hello friend,

    Give a try to the following also. They may help you  as it worked for me.

    1.  ARM9_0: File Loader: Data verification failed at address 0x80000000 Please verify target memory and memory map.

    This can be due to to improper gel file.

    Try loading the latest gel files available from the vendor for your board for your CCS version. Else look at OMAP data sheet, note down the memory locations corresponding to 0x80000000 (shared memory) , make corrections this gel file and save it with different name  and use. It should work.

    2) is there any way that i role back my CPLD version to the orignal thing

    Please contact spectrumdigital regarding this.

    All the best

    Prat