This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ccs project path relative to workspace



Is there a way in CCS 6.1 to add a project to a workspace using a relative path?  I know that you can link resources

using a relative path but I need a relative path for the project itself.

Victor

  • Hi Victor,
    This is not possible. An absolute path to the project is always used by the workspace. Sorry.

    May I ask what you use case is where you would need such functionality?

    Thanks
    ki
  • Hi Ki,

      On our project several hardware engineers use CCS to download the application to a Hercules microprocessor.

    When they check out a specific revision of the code they have to go through creating a workspace and importing

    the project into that workspace.  I was hoping to set it up so that the workspace was part of the code repository

    so they only have to check out the code, switch to the workspace and then build.  The location of

    the workspace on each engineer's computer is not fixed so we want to be able to download the code into any directory

    and use paths relative to that directory.  Of course the exception is the TI tools which are always in the same

    directory.

    Victor

  • I see. Eclipse workspaces are not designed to be part of a code repository. It is a local folder for each user, of which projects are imported to. What is in the workspace that you wish to be shared and preserved?