I'm using Code Composer Studio 4.1.2.00027 and it does now show locals. If I put the cursor over a local it does not show anything. If I look in the Local(1) window the name is there but the value is "identifier not found".
For example I stop the debugger in a method of an object and the "this" pointer value is "identifier not found:this". Is there a setting I need to turn on? This works fine in CCS 3.