Other Parts Discussed in Thread: MSP-TS430RGZ48C, MSP-FET
Hello TI.
Im trying to program a microcontroller using the MSP-FET and a MSP-TS430RGZ48C. On the board I have connected 1 and 2 on J1 to use the supply from the JTAG. However on the MSP-FET the mode diode is red while the Power diode is turned off. When i try to debug in CCS it tells me there is an error initializing emulator and i need to update the firmware. I press update and both diodes on the MSP-FET starts to blink, after a while the update terminates, BUT tells me to update the firmware again? this scenario happens again and again. How to solve this problem?
If i ignore the firmware update it tell me it could not set device Vcc.
Im using CCS 6.1.0
Regards,
Mathias