This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problem with debugging two Concerto with two xds100v2 emulator

Hi,

I am trying to debug two concerto at the same time. I have one computer and two xds100v2 emulators. I can connect to two concerto while changing the serial number of target configurations on advanced target configuration settings. It is ok. But I have a problem with debugging. When I stop one concerto on the CCS window, the other CCS window stops working. I can not debug two concerto at the same time. One of the CCS windows stops running and shows APPCRASH error.

How can I solve this problem?

Thanks.