This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

construction of static objects fails with large/lower/upper

Other Parts Discussed in Thread: MSP430FR6989

The following example

//test.hpp
class test {
public:
	static constexpr unsigned max_count = 16;
	inline test() noexcept {
		add(this);
	}
	static inline unsigned get_count() noexcept {
		return count;
	}
protected:
	static void add(test*) noexcept;
	static test* tests[max_count];
	static unsigned count;
};
//test.cpp
#include "test.hpp"

test t1, t2, t3, t4, t5;

//main.cpp (fragment)
test* test::tests[test::max_count];
unsigned test::count = 0;

void test::add(test* t) {
	if( count >= max_count ) return;
	tests[count++] = t;
}

works as expected when build with msp430-elf-gcc 4.9.1 using options

-mlarge
-mcode-region=none
-mdata-region=none

however, when options are set to

-mlarge
-mcode-region=lower
-mdata-region=upper

test.count contains FF instead of expected 05.

Verbose build log is attached

/opt/ti/ccsv6/utils/bin/gmake -k all 
Building file: ../main.cpp
Invoking: GNU Compiler
"/opt/ti/gcc/bin/msp430-elf-gcc" -c -std=c++1y -mmcu=msp430fr6989 -fno-exceptions -I"/opt/ti/gcc/msp430-elf/include" -I"/opt/ti/ccsv6/ccs_base/msp430/include_gcc" -O3 -Os -Wall -v -mlarge -mcode-region=none -mdata-region=none -MMD -MP -MF"main.d" -MT"main.d" -fno-rtti -o"main.o"  "../main.cpp"
Using built-in specs.
COLLECT_GCC=/opt/ti/gcc/bin/msp430-elf-gcc
Target: msp430-elf
Configured with: /opt/redhat/msp430-14r1-364/sources/tools/configure --host=i686-redhat-linux --build=i686-redhat-linux --target=msp430-elf --prefix=/opt/redhat/msp430-14r1-364/i686-redhat-linux --enable-languages=c,c++
Thread model: single
gcc version 4.9.1 20140707 (prerelease (msp430-14r1-364)) (GNUPro 14r1) (Based on: GCC 4.8 GDB 7.7 Binutils 2.24 Newlib 2.1) (GCC) 
COLLECT_GCC_OPTIONS='-c' '-std=c++1y' '-mmcu=msp430fr6989' '-fno-exceptions' '-I' '/opt/ti/gcc/msp430-elf/include' '-I' '/opt/ti/ccsv6/ccs_base/msp430/include_gcc' '-O3' '-Os' '-Wall' '-v' '-mlarge' '-mcode-region=none' '-mdata-region=none' '-MMD' '-MP' '-MF' 'main.d' '-MT' 'main.d' '-fno-rtti' '-o' 'main.o'
 /opt/ti/gcc/bin/../libexec/gcc/msp430-elf/4.9.1/cc1plus -quiet -v -I /opt/ti/gcc/msp430-elf/include -I /opt/ti/ccsv6/ccs_base/msp430/include_gcc -imultilib large -iprefix /opt/ti/gcc/bin/../lib/gcc/msp430-elf/4.9.1/ -MMD main.d -MF main.d -MP -MT main.d ../main.cpp -quiet -dumpbase main.cpp -mmcu=msp430fr6989 -mlarge -mcode-region=none -mdata-region=none -auxbase-strip main.o -O3 -Os -Wall -std=c++1y -version -fno-exceptions -fno-rtti -o /tmp/ccAmTYji.s
GNU C++ (GCC) version 4.9.1 20140707 (prerelease (msp430-14r1-364)) (GNUPro 14r1) (Based on: GCC 4.8 GDB 7.7 Binutils 2.24 Newlib 2.1) (msp430-elf)
	compiled by GNU C version 4.1.2 20080704 (Red Hat 4.1.2-55), GMP version 5.0.1, MPFR version 3.1.0, MPC version 0.9
GGC heuristics: --param ggc-min-expand=100 --param ggc-min-heapsize=131072
ignoring nonexistent directory "/opt/ti/gcc/bin/../lib/gcc/msp430-elf/4.9.1/../../../../msp430-elf/sys-include"
ignoring duplicate directory "/opt/ti/gcc/bin/../lib/gcc/../../lib/gcc/msp430-elf/4.9.1/../../../../msp430-elf/include/c++/4.9.1"
ignoring duplicate directory "/opt/ti/gcc/bin/../lib/gcc/../../lib/gcc/msp430-elf/4.9.1/../../../../msp430-elf/include/c++/4.9.1/msp430-elf/large"
ignoring duplicate directory "/opt/ti/gcc/bin/../lib/gcc/../../lib/gcc/msp430-elf/4.9.1/../../../../msp430-elf/include/c++/4.9.1/backward"
ignoring duplicate directory "/opt/ti/gcc/bin/../lib/gcc/../../lib/gcc/msp430-elf/4.9.1/include"
ignoring duplicate directory "/opt/ti/gcc/bin/../lib/gcc/../../lib/gcc/msp430-elf/4.9.1/include-fixed"
ignoring nonexistent directory "/opt/ti/gcc/bin/../lib/gcc/../../lib/gcc/msp430-elf/4.9.1/../../../../msp430-elf/sys-include"
ignoring duplicate directory "/opt/ti/gcc/bin/../lib/gcc/../../lib/gcc/msp430-elf/4.9.1/../../../../msp430-elf/include"
ignoring duplicate directory "/opt/ti/gcc/msp430-elf/include"
  as it is a non-system directory that duplicates a system directory
#include "..." search starts here:
#include <...> search starts here:
 /opt/ti/ccsv6/ccs_base/msp430/include_gcc
 /opt/ti/gcc/bin/../lib/gcc/msp430-elf/4.9.1/../../../../msp430-elf/include/c++/4.9.1
 /opt/ti/gcc/bin/../lib/gcc/msp430-elf/4.9.1/../../../../msp430-elf/include/c++/4.9.1/msp430-elf/large
 /opt/ti/gcc/bin/../lib/gcc/msp430-elf/4.9.1/../../../../msp430-elf/include/c++/4.9.1/backward
 /opt/ti/gcc/bin/../lib/gcc/msp430-elf/4.9.1/include
 /opt/ti/gcc/bin/../lib/gcc/msp430-elf/4.9.1/include-fixed
 /opt/ti/gcc/bin/../lib/gcc/msp430-elf/4.9.1/../../../../msp430-elf/include
End of search list.
GNU C++ (GCC) version 4.9.1 20140707 (prerelease (msp430-14r1-364)) (GNUPro 14r1) (Based on: GCC 4.8 GDB 7.7 Binutils 2.24 Newlib 2.1) (msp430-elf)
	compiled by GNU C version 4.1.2 20080704 (Red Hat 4.1.2-55), GMP version 5.0.1, MPFR version 3.1.0, MPC version 0.9
GGC heuristics: --param ggc-min-expand=100 --param ggc-min-heapsize=131072
Compiler executable checksum: 1a1fed4172c6cd7daa4ff072f27c6f2a
COLLECT_GCC_OPTIONS='-c' '-std=c++1y' '-mmcu=msp430fr6989' '-fno-exceptions' '-I' '/opt/ti/gcc/msp430-elf/include' '-I' '/opt/ti/ccsv6/ccs_base/msp430/include_gcc' '-O3' '-Os' '-Wall' '-v' '-mlarge' '-mcode-region=none' '-mdata-region=none' '-MMD' '-MP' '-MF' 'main.d' '-MT' 'main.d' '-fno-rtti' '-o' 'main.o'
 /opt/ti/gcc/bin/../lib/gcc/msp430-elf/4.9.1/../../../../msp430-elf/bin/as -v -I /opt/ti/gcc/msp430-elf/include -I /opt/ti/ccsv6/ccs_base/msp430/include_gcc -mP -mmcu=msp430fr6989 -ml -md -o main.o /tmp/ccAmTYji.s
GNU assembler version 2.24.51 (msp430-elf) using BFD version (GNU Binutils) 2.24.51.20140505
COMPILER_PATH=/opt/ti/gcc/bin/../libexec/gcc/msp430-elf/4.9.1/:/opt/ti/gcc/bin/../libexec/gcc/:/opt/ti/gcc/bin/../lib/gcc/msp430-elf/4.9.1/../../../../msp430-elf/bin/
LIBRARY_PATH=/opt/ti/gcc/bin/../lib/gcc/msp430-elf/4.9.1/large/:/opt/ti/gcc/bin/../lib/gcc/msp430-elf/4.9.1/../../../../msp430-elf/lib/large/:/opt/ti/gcc/bin/../lib/gcc/msp430-elf/4.9.1/:/opt/ti/gcc/bin/../lib/gcc/:/opt/ti/gcc/bin/../lib/gcc/msp430-elf/4.9.1/../../../../msp430-elf/lib/
COLLECT_GCC_OPTIONS='-c' '-std=c++1y' '-mmcu=msp430fr6989' '-fno-exceptions' '-I' '/opt/ti/gcc/msp430-elf/include' '-I' '/opt/ti/ccsv6/ccs_base/msp430/include_gcc' '-O3' '-Os' '-Wall' '-v' '-mlarge' '-mcode-region=none' '-mdata-region=none' '-MMD' '-MP' '-MF' 'main.d' '-MT' 'main.d' '-fno-rtti' '-o' 'main.o'
Finished building: ../main.cpp
 
Building file: ../test.cpp
Invoking: GNU Compiler
"/opt/ti/gcc/bin/msp430-elf-gcc" -c -std=c++1y -mmcu=msp430fr6989 -fno-exceptions -I"/opt/ti/gcc/msp430-elf/include" -I"/opt/ti/ccsv6/ccs_base/msp430/include_gcc" -O3 -Os -Wall -v -mlarge -mcode-region=none -mdata-region=none -MMD -MP -MF"test.d" -MT"test.d" -fno-rtti -o"test.o"  "../test.cpp"
Using built-in specs.
COLLECT_GCC=/opt/ti/gcc/bin/msp430-elf-gcc
Target: msp430-elf
Configured with: /opt/redhat/msp430-14r1-364/sources/tools/configure --host=i686-redhat-linux --build=i686-redhat-linux --target=msp430-elf --prefix=/opt/redhat/msp430-14r1-364/i686-redhat-linux --enable-languages=c,c++
Thread model: single
gcc version 4.9.1 20140707 (prerelease (msp430-14r1-364)) (GNUPro 14r1) (Based on: GCC 4.8 GDB 7.7 Binutils 2.24 Newlib 2.1) (GCC) 
COLLECT_GCC_OPTIONS='-c' '-std=c++1y' '-mmcu=msp430fr6989' '-fno-exceptions' '-I' '/opt/ti/gcc/msp430-elf/include' '-I' '/opt/ti/ccsv6/ccs_base/msp430/include_gcc' '-O3' '-Os' '-Wall' '-v' '-mlarge' '-mcode-region=none' '-mdata-region=none' '-MMD' '-MP' '-MF' 'test.d' '-MT' 'test.d' '-fno-rtti' '-o' 'test.o'
 /opt/ti/gcc/bin/../libexec/gcc/msp430-elf/4.9.1/cc1plus -quiet -v -I /opt/ti/gcc/msp430-elf/include -I /opt/ti/ccsv6/ccs_base/msp430/include_gcc -imultilib large -iprefix /opt/ti/gcc/bin/../lib/gcc/msp430-elf/4.9.1/ -MMD test.d -MF test.d -MP -MT test.d ../test.cpp -quiet -dumpbase test.cpp -mmcu=msp430fr6989 -mlarge -mcode-region=none -mdata-region=none -auxbase-strip test.o -O3 -Os -Wall -std=c++1y -version -fno-exceptions -fno-rtti -o /tmp/cc08nMEq.s
GNU C++ (GCC) version 4.9.1 20140707 (prerelease (msp430-14r1-364)) (GNUPro 14r1) (Based on: GCC 4.8 GDB 7.7 Binutils 2.24 Newlib 2.1) (msp430-elf)
	compiled by GNU C version 4.1.2 20080704 (Red Hat 4.1.2-55), GMP version 5.0.1, MPFR version 3.1.0, MPC version 0.9
GGC heuristics: --param ggc-min-expand=100 --param ggc-min-heapsize=131072
ignoring nonexistent directory "/opt/ti/gcc/bin/../lib/gcc/msp430-elf/4.9.1/../../../../msp430-elf/sys-include"
ignoring duplicate directory "/opt/ti/gcc/bin/../lib/gcc/../../lib/gcc/msp430-elf/4.9.1/../../../../msp430-elf/include/c++/4.9.1"
ignoring duplicate directory "/opt/ti/gcc/bin/../lib/gcc/../../lib/gcc/msp430-elf/4.9.1/../../../../msp430-elf/include/c++/4.9.1/msp430-elf/large"
ignoring duplicate directory "/opt/ti/gcc/bin/../lib/gcc/../../lib/gcc/msp430-elf/4.9.1/../../../../msp430-elf/include/c++/4.9.1/backward"
ignoring duplicate directory "/opt/ti/gcc/bin/../lib/gcc/../../lib/gcc/msp430-elf/4.9.1/include"
ignoring duplicate directory "/opt/ti/gcc/bin/../lib/gcc/../../lib/gcc/msp430-elf/4.9.1/include-fixed"
ignoring nonexistent directory "/opt/ti/gcc/bin/../lib/gcc/../../lib/gcc/msp430-elf/4.9.1/../../../../msp430-elf/sys-include"
ignoring duplicate directory "/opt/ti/gcc/bin/../lib/gcc/../../lib/gcc/msp430-elf/4.9.1/../../../../msp430-elf/include"
ignoring duplicate directory "/opt/ti/gcc/msp430-elf/include"
  as it is a non-system directory that duplicates a system directory
#include "..." search starts here:
#include <...> search starts here:
 /opt/ti/ccsv6/ccs_base/msp430/include_gcc
 /opt/ti/gcc/bin/../lib/gcc/msp430-elf/4.9.1/../../../../msp430-elf/include/c++/4.9.1
 /opt/ti/gcc/bin/../lib/gcc/msp430-elf/4.9.1/../../../../msp430-elf/include/c++/4.9.1/msp430-elf/large
 /opt/ti/gcc/bin/../lib/gcc/msp430-elf/4.9.1/../../../../msp430-elf/include/c++/4.9.1/backward
 /opt/ti/gcc/bin/../lib/gcc/msp430-elf/4.9.1/include
 /opt/ti/gcc/bin/../lib/gcc/msp430-elf/4.9.1/include-fixed
 /opt/ti/gcc/bin/../lib/gcc/msp430-elf/4.9.1/../../../../msp430-elf/include
End of search list.
GNU C++ (GCC) version 4.9.1 20140707 (prerelease (msp430-14r1-364)) (GNUPro 14r1) (Based on: GCC 4.8 GDB 7.7 Binutils 2.24 Newlib 2.1) (msp430-elf)
	compiled by GNU C version 4.1.2 20080704 (Red Hat 4.1.2-55), GMP version 5.0.1, MPFR version 3.1.0, MPC version 0.9
GGC heuristics: --param ggc-min-expand=100 --param ggc-min-heapsize=131072
Compiler executable checksum: 1a1fed4172c6cd7daa4ff072f27c6f2a
COLLECT_GCC_OPTIONS='-c' '-std=c++1y' '-mmcu=msp430fr6989' '-fno-exceptions' '-I' '/opt/ti/gcc/msp430-elf/include' '-I' '/opt/ti/ccsv6/ccs_base/msp430/include_gcc' '-O3' '-Os' '-Wall' '-v' '-mlarge' '-mcode-region=none' '-mdata-region=none' '-MMD' '-MP' '-MF' 'test.d' '-MT' 'test.d' '-fno-rtti' '-o' 'test.o'
 /opt/ti/gcc/bin/../lib/gcc/msp430-elf/4.9.1/../../../../msp430-elf/bin/as -v -I /opt/ti/gcc/msp430-elf/include -I /opt/ti/ccsv6/ccs_base/msp430/include_gcc -mP -mmcu=msp430fr6989 -ml -md -o test.o /tmp/cc08nMEq.s
GNU assembler version 2.24.51 (msp430-elf) using BFD version (GNU Binutils) 2.24.51.20140505
COMPILER_PATH=/opt/ti/gcc/bin/../libexec/gcc/msp430-elf/4.9.1/:/opt/ti/gcc/bin/../libexec/gcc/:/opt/ti/gcc/bin/../lib/gcc/msp430-elf/4.9.1/../../../../msp430-elf/bin/
LIBRARY_PATH=/opt/ti/gcc/bin/../lib/gcc/msp430-elf/4.9.1/large/:/opt/ti/gcc/bin/../lib/gcc/msp430-elf/4.9.1/../../../../msp430-elf/lib/large/:/opt/ti/gcc/bin/../lib/gcc/msp430-elf/4.9.1/:/opt/ti/gcc/bin/../lib/gcc/:/opt/ti/gcc/bin/../lib/gcc/msp430-elf/4.9.1/../../../../msp430-elf/lib/
COLLECT_GCC_OPTIONS='-c' '-std=c++1y' '-mmcu=msp430fr6989' '-fno-exceptions' '-I' '/opt/ti/gcc/msp430-elf/include' '-I' '/opt/ti/ccsv6/ccs_base/msp430/include_gcc' '-O3' '-Os' '-Wall' '-v' '-mlarge' '-mcode-region=none' '-mdata-region=none' '-MMD' '-MP' '-MF' 'test.d' '-MT' 'test.d' '-fno-rtti' '-o' 'test.o'
Finished building: ../test.cpp
 
Building target: uart_echo.out
Invoking: GNU Linker
"/opt/ti/gcc/bin/msp430-elf-gcc" -mmcu=msp430fr6989 -fno-exceptions -O3 -Os -Wall -v -mlarge -Wl,-Map,"uart_echo.map" -mcode-region=none -mdata-region=none -o"uart_echo.out" "./main.o" "./msp430_serial.o" "./test.o" "./driverlib/MSP430FR5xx_6xx/adc12_b.o" "./driverlib/MSP430FR5xx_6xx/aes256.o" "./driverlib/MSP430FR5xx_6xx/comp_e.o" "./driverlib/MSP430FR5xx_6xx/crc.o" "./driverlib/MSP430FR5xx_6xx/crc32.o" "./driverlib/MSP430FR5xx_6xx/cs.o" "./driverlib/MSP430FR5xx_6xx/dma.o" "./driverlib/MSP430FR5xx_6xx/esi.o" "./driverlib/MSP430FR5xx_6xx/eusci_a_spi.o" "./driverlib/MSP430FR5xx_6xx/eusci_a_uart.o" "./driverlib/MSP430FR5xx_6xx/eusci_b_i2c.o" "./driverlib/MSP430FR5xx_6xx/eusci_b_spi.o" "./driverlib/MSP430FR5xx_6xx/framctl.o" "./driverlib/MSP430FR5xx_6xx/gpio.o" "./driverlib/MSP430FR5xx_6xx/lcd_c.o" "./driverlib/MSP430FR5xx_6xx/mpu.o" "./driverlib/MSP430FR5xx_6xx/mpy32.o" "./driverlib/MSP430FR5xx_6xx/pmm.o" "./driverlib/MSP430FR5xx_6xx/ram.o" "./driverlib/MSP430FR5xx_6xx/ref_a.o" "./driverlib/MSP430FR5xx_6xx/rtc_b.o" "./driverlib/MSP430FR5xx_6xx/rtc_c.o" "./driverlib/MSP430FR5xx_6xx/sfr.o" "./driverlib/MSP430FR5xx_6xx/sysctl.o" "./driverlib/MSP430FR5xx_6xx/timer_a.o" "./driverlib/MSP430FR5xx_6xx/timer_b.o" "./driverlib/MSP430FR5xx_6xx/tlv.o" "./driverlib/MSP430FR5xx_6xx/wdt_a.o" -T"../msp430fr6989.ld"  -Wl,--start-group -l"c" -l"gcc" -Wl,--end-group 
Using built-in specs.
COLLECT_GCC=/opt/ti/gcc/bin/msp430-elf-gcc
COLLECT_LTO_WRAPPER=/opt/ti/gcc/bin/../libexec/gcc/msp430-elf/4.9.1/lto-wrapper
Target: msp430-elf
Configured with: /opt/redhat/msp430-14r1-364/sources/tools/configure --host=i686-redhat-linux --build=i686-redhat-linux --target=msp430-elf --prefix=/opt/redhat/msp430-14r1-364/i686-redhat-linux --enable-languages=c,c++
Thread model: single
gcc version 4.9.1 20140707 (prerelease (msp430-14r1-364)) (GNUPro 14r1) (Based on: GCC 4.8 GDB 7.7 Binutils 2.24 Newlib 2.1) (GCC) 
COMPILER_PATH=/opt/ti/gcc/bin/../libexec/gcc/msp430-elf/4.9.1/:/opt/ti/gcc/bin/../libexec/gcc/:/opt/ti/gcc/bin/../lib/gcc/msp430-elf/4.9.1/../../../../msp430-elf/bin/
LIBRARY_PATH=/opt/ti/gcc/bin/../lib/gcc/msp430-elf/4.9.1/large/:/opt/ti/gcc/bin/../lib/gcc/msp430-elf/4.9.1/../../../../msp430-elf/lib/large/:/opt/ti/gcc/bin/../lib/gcc/msp430-elf/4.9.1/:/opt/ti/gcc/bin/../lib/gcc/:/opt/ti/gcc/bin/../lib/gcc/msp430-elf/4.9.1/../../../../msp430-elf/lib/
COLLECT_GCC_OPTIONS='-mmcu=msp430fr6989' '-fno-exceptions' '-O3' '-Os' '-Wall' '-v' '-mlarge' '-mcode-region=none' '-mdata-region=none' '-o' 'uart_echo.out' '-T' '../msp430fr6989.ld'
 /opt/ti/gcc/bin/../libexec/gcc/msp430-elf/4.9.1/collect2 -plugin /opt/ti/gcc/bin/../libexec/gcc/msp430-elf/4.9.1/liblto_plugin.so -plugin-opt=/opt/ti/gcc/bin/../libexec/gcc/msp430-elf/4.9.1/lto-wrapper -plugin-opt=-fresolution=/tmp/ccnfyLKt.res -plugin-opt=-pass-through=-lgcc -plugin-opt=-pass-through=-lc -plugin-opt=-pass-through=-lgcc -plugin-opt=-pass-through=-lcrt -plugin-opt=-pass-through=-lnosys -plugin-opt=-pass-through=-lgcc --gc-sections -o uart_echo.out /opt/ti/gcc/bin/../lib/gcc/msp430-elf/4.9.1/../../../../msp430-elf/lib/large/crt0.o /opt/ti/gcc/bin/../lib/gcc/msp430-elf/4.9.1/large/crtbegin.o -L/opt/ti/gcc/bin/../lib/gcc/msp430-elf/4.9.1/large -L/opt/ti/gcc/bin/../lib/gcc/msp430-elf/4.9.1/../../../../msp430-elf/lib/large -L/opt/ti/gcc/bin/../lib/gcc/msp430-elf/4.9.1 -L/opt/ti/gcc/bin/../lib/gcc -L/opt/ti/gcc/bin/../lib/gcc/msp430-elf/4.9.1/../../../../msp430-elf/lib -Map uart_echo.map ./main.o ./msp430_serial.o ./test.o ./driverlib/MSP430FR5xx_6xx/adc12_b.o ./driverlib/MSP430FR5xx_6xx/aes256.o ./driverlib/MSP430FR5xx_6xx/comp_e.o ./driverlib/MSP430FR5xx_6xx/crc.o ./driverlib/MSP430FR5xx_6xx/crc32.o ./driverlib/MSP430FR5xx_6xx/cs.o ./driverlib/MSP430FR5xx_6xx/dma.o ./driverlib/MSP430FR5xx_6xx/esi.o ./driverlib/MSP430FR5xx_6xx/eusci_a_spi.o ./driverlib/MSP430FR5xx_6xx/eusci_a_uart.o ./driverlib/MSP430FR5xx_6xx/eusci_b_i2c.o ./driverlib/MSP430FR5xx_6xx/eusci_b_spi.o ./driverlib/MSP430FR5xx_6xx/framctl.o ./driverlib/MSP430FR5xx_6xx/gpio.o ./driverlib/MSP430FR5xx_6xx/lcd_c.o ./driverlib/MSP430FR5xx_6xx/mpu.o ./driverlib/MSP430FR5xx_6xx/mpy32.o ./driverlib/MSP430FR5xx_6xx/pmm.o ./driverlib/MSP430FR5xx_6xx/ram.o ./driverlib/MSP430FR5xx_6xx/ref_a.o ./driverlib/MSP430FR5xx_6xx/rtc_b.o ./driverlib/MSP430FR5xx_6xx/rtc_c.o ./driverlib/MSP430FR5xx_6xx/sfr.o ./driverlib/MSP430FR5xx_6xx/sysctl.o ./driverlib/MSP430FR5xx_6xx/timer_a.o ./driverlib/MSP430FR5xx_6xx/timer_b.o ./driverlib/MSP430FR5xx_6xx/tlv.o ./driverlib/MSP430FR5xx_6xx/wdt_a.o --start-group -lc -lgcc --end-group -lgcc --start-group -lc -lgcc -lcrt -lnosys --end-group -lgcc /opt/ti/gcc/bin/../lib/gcc/msp430-elf/4.9.1/large/crtend.o /opt/ti/gcc/bin/../lib/gcc/msp430-elf/4.9.1/../../../../msp430-elf/lib/large/crtn.o -lgcc -T ../msp430fr6989.ld
Finished building target: uart_echo.out
 

**** Build Finished ****