Other Parts Discussed in Thread: TM4C123GH6PM
Hi, I searched the forum and there are several posts related to this problem, but no single method to answer the issue once and for all. It happens randomly when I change the source code of examples I am working on. The error itself is random too, with the memory address changing and sometimes not even shown.
My environment is the following:
CCS for Mac OS version 6.1.1.00028
Launchpad TM4C123G with a Tiva TM4C123GH6PM
Digilent Orbit Boosterpack
Stellaris ICDI
Mac OS X 10.10.5 Yosemite
The error happens after I change the code, often when I remove code that I do not want to keep. When I debug and step into the code I can see one pointer change from this
pbFont unsigned char * 0x000031F3 "\275\255\361\010\015\001\221" (Hex) 0x200004EC
to this
pbFont unsigned char * 0x202020B0 (Hex) 0x200004EC
This is the GEL file
menuitem "StartUp"
hotmenu StartUp()
{
/* Load the CortexM3_util.gel file */
GEL_LoadGel("$(GEL_file_dir)/CortexM3_util.gel");
GEL_MapOff();
GEL_MapReset();
GEL_MapOn();
memorymap_init();
}
OnTargetConnect()
{
}
memorymap_init()
{
/*
* Syntax for GEL_MapAddStr.
* GEL_MapAddStr(address, page, length, "attribute", waitstate);
Basic Attribute Types Derived Attribute Types
String Description String Description
R Read NONE No memory/protected
W Write RAM Read and write
P Port ROM Read only
EX External WOM Write only
EM Emulator INPORT Port read only
PR Programmable OUTPORT Port write only
ER Erasable IOPORT Port read and write
DA Dual access SARAM Single access RAM
ASn Access size DARAM Dual access RAM
SHnC Shared FLASH Flash ROM
CACHE Cache EXRAM External RAM
TX Text EXROM External ROM
MN Monitor EPROM Erasable write-able EPROM
SA Single access MONITOR Monitor ROM
FL Flash PRAM Program RAM
MR Memory mapped PROM Program ROM
NULL NULL NULL NULL
*/
GEL_MapAddStr(0x00000000, 0, 0x00040000, "R", 0); /* Flash */
GEL_MapAddStr(0x01000000, 0, 0x00008c00, "R", 0); /* ROM */
GEL_MapAddStr(0x20000000, 0, 0x00008000, "R|W", 0); /* SRAM */
GEL_MapAddStr(0x40000000, 0, 0x00001000, "R|W", 0); /* WATCHDOG0 */
GEL_MapAddStr(0x40001000, 0, 0x00001000, "R|W", 0); /* WATCHDOG1 */
GEL_MapAddStr(0x40004000, 0, 0x00001000, "R|W", 0); /* GPIO PORTA */
GEL_MapAddStr(0x40005000, 0, 0x00001000, "R|W", 0); /* GPIO PORTB */
GEL_MapAddStr(0x40006000, 0, 0x00001000, "R|W", 0); /* GPIO PORTC */
GEL_MapAddStr(0x40007000, 0, 0x00001000, "R|W", 0); /* GPIO PORTD */
GEL_MapAddStr(0x40008000, 0, 0x00001000, "R|W", 0); /* SSI0 */
GEL_MapAddStr(0x40009000, 0, 0x00001000, "R|W", 0); /* SSI1 */
GEL_MapAddStr(0x4000A000, 0, 0x00001000, "R|W", 0); /* SSI2 */
GEL_MapAddStr(0x4000B000, 0, 0x00001000, "R|W", 0); /* SSI3 */
GEL_MapAddStr(0x4000C000, 0, 0x00001000, "R|W", 0); /* UART0 */
GEL_MapAddStr(0x4000D000, 0, 0x00001000, "R|W", 0); /* UART1 */
GEL_MapAddStr(0x4000E000, 0, 0x00001000, "R|W", 0); /* UART2 */
GEL_MapAddStr(0x4000F000, 0, 0x00001000, "R|W", 0); /* UART3 */
GEL_MapAddStr(0x40010000, 0, 0x00001000, "R|W", 0); /* UART4 */
GEL_MapAddStr(0x40011000, 0, 0x00001000, "R|W", 0); /* UART5 */
GEL_MapAddStr(0x40012000, 0, 0x00001000, "R|W", 0); /* UART6 */
GEL_MapAddStr(0x40013000, 0, 0x00001000, "R|W", 0); /* UART7 */
GEL_MapAddStr(0x40020000, 0, 0x00001000, "R|W", 0); /* I2C0 */
GEL_MapAddStr(0x40021000, 0, 0x00001000, "R|W", 0); /* I2C1 */
GEL_MapAddStr(0x40022000, 0, 0x00001000, "R|W", 0); /* I2C2 */
GEL_MapAddStr(0x40023000, 0, 0x00001000, "R|W", 0); /* I2C3 */
GEL_MapAddStr(0x40024000, 0, 0x00001000, "R|W", 0); /* GPIO PORTE */
GEL_MapAddStr(0x40025000, 0, 0x00001000, "R|W", 0); /* GPIO PORTF */
GEL_MapAddStr(0x40028000, 0, 0x00001000, "R|W", 0); /* PWM0 */
GEL_MapAddStr(0x40029000, 0, 0x00001000, "R|W", 0); /* PWM1 */
GEL_MapAddStr(0x4002C000, 0, 0x00001000, "R|W", 0); /* QEI0 */
GEL_MapAddStr(0x4002D000, 0, 0x00001000, "R|W", 0); /* QEI1 */
GEL_MapAddStr(0x40030000, 0, 0x00001000, "R|W", 0); /* TIMER0 */
GEL_MapAddStr(0x40031000, 0, 0x00001000, "R|W", 0); /* TIMER1 */
GEL_MapAddStr(0x40032000, 0, 0x00001000, "R|W", 0); /* TIMER2 */
GEL_MapAddStr(0x40033000, 0, 0x00001000, "R|W", 0); /* TIMER3 */
GEL_MapAddStr(0x40034000, 0, 0x00001000, "R|W", 0); /* TIMER4 */
GEL_MapAddStr(0x40035000, 0, 0x00001000, "R|W", 0); /* TIMER5 */
GEL_MapAddStr(0x40036000, 0, 0x00001000, "R|W", 0); /* WTIMER0 */
GEL_MapAddStr(0x40037000, 0, 0x00001000, "R|W", 0); /* WTIMER1 */
GEL_MapAddStr(0x40038000, 0, 0x00001000, "R|W", 0); /* ADC0 */
GEL_MapAddStr(0x40039000, 0, 0x00001000, "R|W", 0); /* ADC1 */
GEL_MapAddStr(0x4003C000, 0, 0x00001000, "R|W", 0); /* COMP */
GEL_MapAddStr(0x40040000, 0, 0x00001000, "R|W", 0); /* CAN0 */
GEL_MapAddStr(0x40041000, 0, 0x00001000, "R|W", 0); /* CAN1 */
GEL_MapAddStr(0x4004C000, 0, 0x00001000, "R|W", 0); /* WTIMER2 */
GEL_MapAddStr(0x4004D000, 0, 0x00001000, "R|W", 0); /* WTIMER3 */
GEL_MapAddStr(0x4004E000, 0, 0x00001000, "R|W", 0); /* WTIMER4 */
GEL_MapAddStr(0x4004F000, 0, 0x00001000, "R|W", 0); /* WTIMER5 */
GEL_MapAddStr(0x40050000, 0, 0x00001000, "R|W", 0); /* USB0 */
GEL_MapAddStr(0x40058000, 0, 0x00001000, "R|W", 0); /* GPIO PORTA AHB */
GEL_MapAddStr(0x40059000, 0, 0x00001000, "R|W", 0); /* GPIO PORTB AHB */
GEL_MapAddStr(0x4005A000, 0, 0x00001000, "R|W", 0); /* GPIO PORTC AHB */
GEL_MapAddStr(0x4005B000, 0, 0x00001000, "R|W", 0); /* GPIO PORTD AHB */
GEL_MapAddStr(0x4005C000, 0, 0x00001000, "R|W", 0); /* GPIO PORTE AHB */
GEL_MapAddStr(0x4005D000, 0, 0x00001000, "R|W", 0); /* GPIO PORTF AHB */
GEL_MapAddStr(0x400AF000, 0, 0x00001000, "R|W", 0); /* EEPROM */
GEL_MapAddStr(0x400F9000, 0, 0x00001000, "R|W", 0); /* SYSEXC */
GEL_MapAddStr(0x400FC000, 0, 0x00001000, "R|W", 0); /* HIB */
GEL_MapAddStr(0x400FD000, 0, 0x00001000, "R|W", 0); /* FLASH CTRL */
GEL_MapAddStr(0x400FE000, 0, 0x00001000, "R|W", 0); /* SYSCTL */
GEL_MapAddStr(0x400FF000, 0, 0x00001000, "R|W", 0); /* UDMA */
GEL_MapAddStr(0x60000000, 0, 0x80000000, "R|W", 0); /* EPI Window (if Enabled) */
GEL_MapAddStr(0xE000E000, 0, 0x00001000, "R|W", 0); /* NVIC */
GEL_TextOut("\nMemory Map Initialization Complete\n");
}
I can't see a way to solve this problem. I will be very grateful for any guidance and enlightenment I can be provided. I am very new to Code Composer and I admit to have a limited knowledge of it.
Regards,
Angelo