Hello,
I have just updated to the latest version of CCS (6.1.1) and also included the MSP ware drivers. I still cannot create a new project or import examples to an existing project for this hardware. It does not show up in the target ring control. I do however see a "Custom MSP432" option. I realize I am a beginner but this is the most frustrating experience I have had with an IDE. I will not use Energia so please do not refer that as an answer.
MSP432P401R Launchpad
Windows 7 x64
CCS 6.1.1.00022
I appreciate any help in resolving this issue.
Thanks,
Chris