Dear readers ,
i get this warning when i build my project ,warning #10424-D: Linker command file , i have searched for the solutions and i find that i must upgrade my linker command files , i am usnig CCS v6.1 , any help plzzz , 
Regards
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear readers ,
i get this warning when i build my project ,warning #10424-D: Linker command file , i have searched for the solutions and i find that i must upgrade my linker command files , i am usnig CCS v6.1 , any help plzzz , 
Regards
Thanks. I can reproduce the issue. The cmd file for the example is out of date. I had to tweak it myself to get it to work. Can you try the attached file with your project?
https://e2e.ti.com/cfs-file/__key/communityserver-discussions-components-files/81/lnk_5F00_msp430f5438a_5F00_mod.cmd
That's odd, the build works perfectly for me with the new cmd file:
'Building target: MSP-EXP430F5438UserExperience.out'
'Invoking: MSP430 Linker'
"C:/ti/ccsv6.1.1.00022/ccsv6/tools/compiler/ti-cgt-msp430_4.4.6/bin/cl430" -vmspx --code_model=large --data_model=large -O2 --opt_for_speed=5 -g --define=__MSP430F5438A__ --diag_warning=225 --display_error_number --silicon_errata=CPU21 --silicon_errata=CPU22 --silicon_errata=CPU23 --silicon_errata=CPU40 --printf_support=minimal -z --stack_size=160 -m"MSP-EXP430F5438UserExperience.map" --heap_size=160 --use_hw_mpy=F5 -i"C:/ti/ccsv6.1.1.00022/ccsv6/tools/compiler/ti-cgt-msp430_4.4.6/lib" -i"C:/ti/ccsv6.1.1.00022/ccsv6/tools/compiler/ti-cgt-msp430_4.4.6/include" -i"C:/ti/ccsv6.1.1.00022/ccsv6/ccs_base/msp430/include" -i"C:/ti/ccsv6.1.1.00022/ccsv6/msp430/include" -i"C:/ti/ccsv6.1.1.00022/ccsv6/tools/compiler/ti-cgt-msp430_4.4.6/lib" -i"C:/ti/ccsv6.1.1.00022/ccsv6/tools/compiler/ti-cgt-msp430_4.4.6/include" --reread_libs --warn_sections --xml_link_info="link_details.xml" --rom_model -o "MSP-EXP430F5438UserExperience.out" "./main.obj" "./system_pre_init.obj" "./UserExperienceDemo/5xx_ACTIVE_test.obj" "./UserExperienceDemo/FFT.obj" "./UserExperienceDemo/FFT_430.obj" "./UserExperienceDemo/LPM.obj" "./UserExperienceDemo/PMM.obj" "./UserExperienceDemo/PowerTest.obj" "./UserExperienceDemo/UserExperienceGraphics.obj" "./UserExperienceDemo/UserExperience_F5438A.obj" "./UserExperienceDemo/adcTemp.obj" "./UserExperienceDemo/audio.obj" "./UserExperienceDemo/balanceBall.obj" "./UserExperienceDemo/clock.obj" "./UserExperienceDemo/flashUtils.obj" "./UserExperienceDemo/menuSetting.obj" "./UserExperienceDemo/usbTest.obj" "./MSP-EXP430F5438_HAL/hal_adc.obj" "./MSP-EXP430F5438_HAL/hal_board.obj" "./MSP-EXP430F5438_HAL/hal_buttons.obj" "./MSP-EXP430F5438_HAL/hal_lcd.obj" "./MSP-EXP430F5438_HAL/hal_lcd_fonts.obj" "./MSP-EXP430F5438_HAL/hal_rf.obj" "./MSP-EXP430F5438_HAL/hal_rtc.obj" "./MSP-EXP430F5438_HAL/hal_usb.obj" "./F5xx_F6xx_Core_Lib/HAL_FLASH.obj" "./F5xx_F6xx_Core_Lib/HAL_PMAP.obj" "./F5xx_F6xx_Core_Lib/HAL_PMM.obj" "./F5xx_F6xx_Core_Lib/HAL_TLV.obj" "./F5xx_F6xx_Core_Lib/HAL_UCS.obj" "../lnk_msp430f5438a_mod.cmd" -l"libc.a"
<Linking>
'Finished building target: MSP-EXP430F5438UserExperience.out'
' '
'Create flash image: TI-TXT'
"C:/ti/ccsv6.1.1.00022/ccsv6/tools/compiler/ti-cgt-msp430_4.4.6/bin/hex430.exe" --ti_txt "MSP-EXP430F5438UserExperience.out" -o "MSP-EXP430F5438UserExperience.txt" -order MS -romwidth 16
Translating to TI-TXT format...
"MSP-EXP430F5438UserExperience.out" .text ==> .text
"MSP-EXP430F5438UserExperience.out" .const ==> .const
"MSP-EXP430F5438UserExperience.out" .text:_isr ==> .text:_isr
"MSP-EXP430F5438UserExperience.out" .cinit ==> .cinit
"MSP-EXP430F5438UserExperience.out" RTC ==> RTC
"MSP-EXP430F5438UserExperience.out" PORT2 ==> PORT2
"MSP-EXP430F5438UserExperience.out" USCI_B3 ==> USCI_B3
"MSP-EXP430F5438UserExperience.out" USCI_A3 ==> USCI_A3
"MSP-EXP430F5438UserExperience.out" USCI_B1 ==> USCI_B1
"MSP-EXP430F5438UserExperience.out" USCI_A1 ==> USCI_A1
"MSP-EXP430F5438UserExperience.out" PORT1 ==> PORT1
"MSP-EXP430F5438UserExperience.out" TIMER1_A1 ==> TIMER1_A1
"MSP-EXP430F5438UserExperience.out" TIMER1_A0 ==> TIMER1_A0
"MSP-EXP430F5438UserExperience.out" DMA ==> DMA
"MSP-EXP430F5438UserExperience.out" USCI_B2 ==> USCI_B2
"MSP-EXP430F5438UserExperience.out" USCI_A2 ==> USCI_A2
"MSP-EXP430F5438UserExperience.out" TIMER0_A1 ==> TIMER0_A1
"MSP-EXP430F5438UserExperience.out" TIMER0_A0 ==> TIMER0_A0
"MSP-EXP430F5438UserExperience.out" ADC12 ==> ADC12
"MSP-EXP430F5438UserExperience.out" USCI_B0 ==> USCI_B0
"MSP-EXP430F5438UserExperience.out" USCI_A0 ==> USCI_A0
"MSP-EXP430F5438UserExperience.out" WDT ==> WDT
"MSP-EXP430F5438UserExperience.out" TIMER0_B1 ==> TIMER0_B1
"MSP-EXP430F5438UserExperience.out" TIMER0_B0 ==> TIMER0_B0
"MSP-EXP430F5438UserExperience.out" UNMI ==> UNMI
"MSP-EXP430F5438UserExperience.out" SYSNMI ==> SYSNMI
"MSP-EXP430F5438UserExperience.out" .reset ==> .reset
' '
**** Build Finished ****