Other Parts Discussed in Thread: TMS320F2812
I'm using: System: TMS320F2812; CCS 5.2.1; DSP/BIOS 5.41.13.42
After my build finishes I get the following error:
gmake: Target `all' not remade because of errors.
**** Build Finished ****
However there are no errors listed in the problems window. Also, the console window won't let me scroll back to the beginning. Is there a way to output the console to a file so I can see all the text? Or increase the console buffer? Also, why won't it list the errors it says it found?