This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Trying to configure CCS v3.3 for XDS510PP TMS320C6415

Other Parts Discussed in Thread: TMS320C6415

OS: Windows XP, CCS v3.3  XDS510PP Plus

I'm trying to configure CCS for a TMS320C6415, but Code Composer Setup doesn't list the C4xx Family as an option.  I can validate the connection to the DSP via SDConfig, but I can't seem to get CCS configured properly.

When I initiate CCS, I get an error message that the "TMS320C64XX is not supported.  Please re-install Code Composer or select a different driver"

 By importing  the c64xx_pp_emulator_0x378.ccs" file, the "sdgov6400_11.dvr" driver file is specified in the setup file,which appears to be the correct driver, and CCS v3.3 should support this device, but there is still a configuration issue.

I've tried using CCS v6.0 previously, didn't have success with it either.  It had issues with the .gel file and I suspect it captures errors in memory configuration that I would need to straighten out to upgrade.