This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

request for technical inquire for CCSv6

I writing to inquire about CCSv6 IDE tool.

 

I Have a problems with CCSv6. (Code Composer Studio, version:6.1.1.00022, Full License)

development Environment: Windows 7 professional KN, Intel® Core™ i5- 4590 CPU @ 3.30GHZ, RAM: 4GB, x64

 

I always getting error messages. When error message is occurred I must stopped the work(Collecting 1,2,3). And restart program. But Its not solution.

The same thing if I restart the program. Time goes by I received the error message like(Collecting 1,2,3)

 

when I open the CCS keep getting error messages. (Like attached image)
The message text is ‘ Collecting garbage(image 1) ’, Internal error(image 2) ’, Problem  Occurred(image 3) . (alarm in the order named)

just, open IDE Tool(CCSv6) but any project is not started(any project is not running).

 

Searching many times related error message. And try to Windows Task Manager(image 4).

Similarly just open IDE Tool(CCSv6) then I see the process view(attached image 4) in Windows Task Manager

 

Surprisingly number of Thread handler has increased as time goes on. Just open the IDE Tool. No give the execution command. any project was not stared.

 

I wonder this work. What can I do for fix the error messages.