This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCSTUDIO

Other Parts Discussed in Thread: CCSTUDIO, CONTROLSUITE

Hello,

My customer is using the CCSTUDIO version 6.0.1.00040 on a computer with an i7 processor and 12GB of RAM.  Every time she tries to build and rebuild her code, it take longer and longer.  When she starts her PC, the first time she builds, it only takes 30sec to complete and gradually that increases to 3min for the same code.  They have also re-installed the control suite.  Any suggestions?

Thanks,

Mehrdad.

  • Hi Mehrdad,

    Can you try upgrading to 6.1.1 ?

    Regards,
    Gautam
  • Mehrdad Bradaran said:
    Every time she tries to build and rebuild her code, it take longer and longer.  When she starts her PC, the first time she builds, it only takes 30sec to complete and gradually that increases to 3min for the same code.

    Mehrdad,

    Can you provide some additional details?
    Does this happen with all projects or only when building specific projects? Are they building a ControlSuite example or their own custom project? Does it hang up at a particular point in the build, or does it just generally slow down overall?

    It wouldn't hurt to try CCS 6.1.1 to check if the issue persists. http://processors.wiki.ti.com/index.php/Download_CCS

    They can simply install CCS 6.1.1 to a different folder, and be able to use CCS 6.0.1 and 6.1.1 side by side, and check the build times on both versions.