When used CCS 6.1.1.00022 with Sitara device support 1.2.5 to create a target configuration file for an AM5728_RevA the following errors were reported for the target configuration file:
Description Resource Path Location Type More than one cpu is named ICECrusherCS_0 AM5728_RevA.ccxml /am5728_hello/targetConfigs Blackhawk USB560-M Emulator, 20-pin JTAG Cable\ICECrusherCS_0 Problem More than one cpu is named ICECrusherCS_0 AM5728_RevA.ccxml /am5728_hello/targetConfigs Blackhawk USB560-M Emulator, 20-pin JTAG Cable\ICECrusherCS_0 Problem More than one cpu is named ICECrusherCS_0 AM5728_RevA.ccxml /am5728_hello/targetConfigs Blackhawk USB560-M Emulator, 20-pin JTAG Cable\ICECrusherCS_0 Problem
The error appears to be caused by the ccsv6/ccs_base/common/targetdb/devices/AM5728_RevA.xml containing four CPUs named ICECrusherCS_0, as components of the IPUs.
Note that this is not currently causing me a problem, but just noticed the error when investigating something else.