This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I am using the C2000 v6.4.9 with -O4 and -mf5.
The #pragma FUNC_ALWAYS_INLINE is not causing the member functions to be inlined. One of the member functions is shown below. What am I doing wrong?
stephen
#pragma FUNC_ALWAYS_INLINE __inline void Ssa::vWrite(SSA_ADDRESS Addr, SSADATA * ptData, U16 u16NumberOfItems) { U16 i; SSADATA * ptMemLoc = (SSADATA*) (SSA_BASE_ADDRESS + Addr); for (i = 0; i < u16NumberOfItems; i++, ptMemLoc++) { ptMemLoc[i] = ptData[i]; } }
The TMS320C28x Optimizing C/C++ Compiler User's Guide documentation for FUNC_ALWAYS_INLINE says:
However, from a search of the User's Guide I can't find a definition of what makes a function legal to inline.The FUNC_ALWAYS_INLINE pragma instructs the compiler to always inline the named function. The compiler only inlines the function if it is legal to inline the function and the compiler is invoked with any level of optimization (--opt_level=0).
Maybe using the --optimizer_interlist option will cause the optimizer to comment on why the function can't be inlined.
I tried repeating the problem with a C version of that function, but so far haven't managed to repeat the problem in that the function is inlined. Are you able to post a complete stand-alone project which shows the problem?stevenh said:The #pragma FUNC_ALWAYS_INLINE is not causing the member functions to be inlined.
Not sure if it is the cause of the problem, but that loop structure looks strange since it is incrementing both ptMemLoc and i each iteration, and also writing to ptMemLoc[i] on each iteration. Is the loop structure intentional?stevenh said:for (i = 0; i < u16NumberOfItems; i++, ptMemLoc++)
{
ptMemLoc[i] = ptData[i];
}
You're correct. I shouldn't be incrementing ptMemLoc.
I removed ", ptMemLoc++" and it still doesn't inline the function
Thanks,
Stephen
When I tried a clean build of that project in CCS 6.1.1 using compiler v6.4.9 got linker errors:stevenh said:The following attached project has the issue.
<Linking> warning #10210-D: creating ".esysmem" section with default size of 0x400; use the -heap option to change the default size undefined first referenced symbol in file --------- ---------------- Ssa::vWrite(unsigned long, unsigned int) <whole-program> error #10234-D: unresolved symbols remain error #10010: errors encountered during linking; "TestCompile2.out" not built >> Compilation failure
The linker errors is due to the declaration of Ssa::vWrite in SsaClass.h not being marked as __inline, but the definition of Ssa::vWrite in SsaClass.cpp being marked as __inline.
Hello Chester,
I changed the declaration, as shown below, and the linker still generates the undefined symbol error.
Stephen
class Ssa { public: Ssa(void); void vInit(void); __inline void vWrite(SSA_ADDRESS tAddress,SSADATA tData); __inline SSADATA tRead(SSA_ADDRESS tAddress); };
For inlining to work the declaration and definition should be marked as __inline and the definition needs to be visible to the users of the class.Chester Gillon said:The linker errors is due to the declaration of Ssa::vWrite in SsaClass.h not being marked as __inline, but the definition of Ssa::vWrite in SsaClass.cpp being marked as __inline.
I have modified the example, which is re-attached 8203.TestCompile2.zip
Looking at the assembler listing in SsaTests.asm shows the ssa.vWrite() call has been inlined:
$C$L1: MOVW DP,#_tData ; [CPU_U] .dwpsn file "../SsaTests.cpp",line 19,column 13,is_stmt,isa 0 ;---------------------------------------------------------------------- ; 19 | ssa.vWrite((SSA_ADDRESS) S1_ADDRESS, tData); ;---------------------------------------------------------------------- MOV AL,@_tData ; [CPU_] |19| .dwpsn file "../SsaClass.h",line 24,column 5,is_stmt,isa 0 MOV *(0:0x5000),AL ; [CPU_] |24| .dwpsn file "../SsaTests.cpp",line 17,column 21,is_stmt,isa 0 BF $C$L1,UNC ; [CPU_] |17| ; branch occurs ; [] |17|