Team,
Am working on Microsoft azure example project.
..\azure-iot-sdks\c\serializer\samples\simplesample_http
When I build the above path example file, I'm getting following error:
"../../simplesample_http.c", line 72: warning: function "sendMessage" was declar
ed but never referenced
building simplesample_http.out ..
<Linking>
warning: automatic library build: using library
"C:\ti\ti-cgt-arm_5.2.5\lib\rtsv7M4_T_le_eabi.lib" for the first time, so it
must be built. This may take a few minutes.
>> ERROR: mklib: could not find program "gmake", required for building libraries
. Modify the PATH environment variable to contain a directory containing this p
rogram.
warning: automatic RTS selection: resolving index library "libc.a" to
"rtsv7M4_T_le_eabi.lib", but "rtsv7M4_T_le_eabi.lib" was not found
undefined first referenced
symbol in file
--------- ----------------
__TI_decompress_none
__TI_decompress_rle24
__TI_zero_init
__aeabi_lmul D:\Users\Rajesh\POC_thermo\test\azure-iot-sdks\c\serializ
er\samples\simplesample_http\tirtos\cc3200\main\package\cfg\main_pem4.src\sysbio
s\sysbios.aem4<BIOS.obj>
__aeabi_uidivmod C:\ti\tirtos_simplelink_2_14_01_20\products\bios_6_42_02_
29\packages\ti\targets\arm\rtsarm\lib\ti.targets.arm.rtsarm.aem4<System.oem4>
__aeabi_uldivmod C:/ti/tirtos_simplelink_2_14_01_20/packages/ti/drivers/li
b/drivers_ccware.aem4<PowerCC3200.oem4>
_args_main C:\ti\tirtos_simplelink_2_14_01_20\products\bios_6_42_02_
29\packages\ti\targets\arm\rtsarm\lib\boot.aem4<boot.oem4>
_nop D:\Users\Rajesh\POC_thermo\test\azure-iot-sdks\c\serializ
er\samples\simplesample_http\tirtos\cc3200\main\package\cfg\main_pem4.oem4
_register_lock D:\Users\Rajesh\POC_thermo\test\azure-iot-sdks\c\serializ
er\samples\simplesample_http\tirtos\cc3200\main\package\cfg\main_pem4.oem4
_register_unlock D:\Users\Rajesh\POC_thermo\test\azure-iot-sdks\c\serializ
er\samples\simplesample_http\tirtos\cc3200\main\package\cfg\main_pem4.oem4
abort C:\ti\tirtos_simplelink_2_14_01_20\products\bios_6_42_02_
29\packages\ti\targets\arm\rtsarm\lib\ti.targets.arm.rtsarm.aem4<System.oem4>
copy_in C:\ti\tirtos_simplelink_2_14_01_20\products\bios_6_42_02_
29\packages\ti\targets\arm\rtsarm\lib\auto_init.aem4<auto_init.oem4>
exit C:\ti\tirtos_simplelink_2_14_01_20\products\bios_6_42_02_
29\packages\ti\targets\arm\rtsarm\lib\ti.targets.arm.rtsarm.aem4<System.oem4>
main_func_sp C:\ti\tirtos_simplelink_2_14_01_20\products\bios_6_42_02_
29\packages\ti\targets\arm\rtsarm\lib\boot.aem4<boot.oem4>
memcpy simplesample_http.o
memset D:\Users\Rajesh\POC_thermo\test\azure-iot-sdks\c\serializ
er\samples\simplesample_http\tirtos\cc3200\main\package\cfg\main_pem4.oem4
strlen netwifi.o
error: unresolved symbols remain
error: errors encountered during linking; "simplesample_http.out" not built
>> Compilation failure
gmake: *** [simplesample_http.out] Error 1
I opened the folder C:\ti\ti-cgt-arm_5.2.5\lib\.. but not able to find the file "rtsv7M4_T_le_eabi.lib".
Can any one help me in resolving this error.