This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS 4.1.1 Install issue - idecore

I have some problems installing Code Composer. I have downloaded the (free) version, and started the install. Everything goes well up until the install of the module called "idecore". Microsoft complains with this message:

"IDE Core 4.1.1.N201003161800 Setup has encountered a problem and needs to close.  We are sorry for the inconvenience."

I selected "MSP430 only" for the install. I have de-installed and re-installed a few times with same result (and some re-boots). A co-worker with the same download file has no problem with the install, so I know the download file is fine. If I drill down the subdirectories to intall_images -> ccscore I can create the same error by running "idecore_setup_4.1.1.N201003161800.exe"

I'm running on Windows XP, service pack 3, Dell Latitude E6400, Intel Core2 Duo CPU, 3.48G RAM. There are no special characters in the path.

Any thoughts where to go to next?

Thanks,

-Steve Reames