Other Parts Discussed in Thread: TMS320DM642, CCSTUDIO
Hello. I have the CCS v3.3 Platinum and DM642 board. The software that came with the shipped package is TMS320DM642 EVM Software CD-ROM for use with CCS 3.1. Then I can't run any example basically because 3.1 comes with .cdb and 3.3 comes with .tcf dsp/bios config file.
I've made some updates, I've installed DSP/BIOS 5.31.02, C6000 CSL version 2.31.00.13, but when I try to build the examples there is always a linking error.
Then I need the DM642 software for CCS v3.3. I haven't found in SpectrumDigital web a link to download it or an email to write to. Whan can I do to start working with this DSP?
Thanx.
Ed.