Hello Chris, Trey, Gautam, and all!
After sometimes, here I am again :)
I have question about modifying Target Configuration for GUI Composer (InstaSPIN_UNIVERSAL.exe).
My board is using F28027F. And to connect with the debugger (XDS100v2), I need to change The JTAG TCLK Frequency to be slower. Please see this screenshot below. If not, the Test connection will be failed.
For InstaSPIN_UNIVERSAL.exe, I can edit .appsettings but it will not help. There is no setting for this JTAG TCLK Frequency.
Actually is it possible to be done or not?
I think I cannot connect my board to InstaSPIN_UNIVERSAL GUI because of this reason so that's why I want to modify this configuration for the GUI (if it is really possible).
Thank you so much for the help.
Have a nice year 2016!
Best regards,
Maria