This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ccsv6.1.2 with fedora 23 linux

Hello All,


I am trying to install ccsv6.1.2 under a fresh install of Fedora 23 and am having no luck.

I tried installing the dependencies are described here:

http://processors.wiki.ti.com/index.php/Linux_Host_Support_CCSv6#Fedora_22_64bit_.28preliminary_don.27t_use_yet.29

but I get the following error from dnf: Error: package cairo-1.14.2-2.fc23.i686 requires libfreetype.so.6, but none of the providers can be installed

I realize these instructions are for Fedora 22 and not Fedora 23, but I'm using them since there are no instructions for Fedora 23 and Fedora 22 is the closest.

I also tried just running the binary that is provided (ccs_setup_6.1.2.00015.bin) but it appears the binary does nothing, i.e., it just returns immediately to the command line.

I could go search for a repo (rpmfusion?) to find libfreetype.so.6, but I thought I'd inquire first if anyone has been successful installing under Fedora 23.

--Randy