This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Disassembly window displays "Unable to retrieve disassembly data from backend"

I'm using CCS V6.1.2.00015 on Fedora 23. I'm using the XDS100V2 debugger. My target is a BeagleBone Black and I am using the BeagleBoneBlack board for my target configuration.

The problem is that after I run my code, I cannot display disassembly at certain locations. The disassembly window displays "Unable to retrieve disassembly data from backend". See a screenshot here:

How can I display the disassembly of my code?

  • PS: This only happens sometimes, not all the time. When I first load the program, these program locations can be disassembled without a problem.
  • Hi Randy,
    Sorry for the delay. It looks to be a potential bug with the disassembly view. If you close and reopen the view, does the issue go away?

    Also, can you provide the program you are using?

    Thanks
    ki