Other Parts Discussed in Thread: MATHLIB
Posted this on TI RTOS forum and was asked to post it here... I am having a problem with the c66x imglib installations on Linux and Windows (CCS 6.1.2) as follows:
xdctools_3_31_02_38_core (33 and 24 are also installed but not referenced by projects)
CCS 6.1.2
Linux:
imglib_c66x_3_1_1_0: Installs and works properly, image_processing demo on AM572x EVM built and tested fine.
imglib_c66x_3_2_0_1: Installs but not discovered. Trying to add using Windows->Preferences...->RTSC did not work (see imglib_c66x_3_1_1_0 under Windows 10 on how attempted to set as 'other Repository' as well).
Windows 10 64 bit:
imglib_c66x_3_1_1_0: Installs but not automatically discovered by CCS, had to go to Windows->Preferences...->RTSC and add it as other Repository and then it automatically added it correctly under IMGLIB C66X. Had to manually extract components archive and drop ti/imglib into imglib_c66x_3_1_1_0\inc to build properly. After changed imported image_processing demo for AM572x EVM built fine for ARM and DSPs other than a .cfg issue with loadCapsule (see other posts).
imglib_c66x_3_2_0_1: Installs but not discovered. Trying to add using Windows->Preferences...->RTSC did not work.
Am installing in same sub-directory area as all the other components, C:\ti on Windows and /home/user/ti on Linux. Numerous other component installs were automatically discovered by CCS. Microsoft Security Essential is the virus protection environment on Windows and it was disabled during install but given have the same problem on Linux it probably has nothing to do with that.
Installed components in ti directory:
bios_6_42_02_29
ctoolslib_2_0_0_0
dsplib_c66x_3_4_0_0
edma3_lld_02_12_01_22
framework_components_3_40_01_04
imglib_c66x_3_1_1_0
imglib_c66x_3_2_0_1
ipc_3_40_01_08
mathlib_c66x_3_1_1_0
ndk_2_24_03_35
pdk_am57xx_1_0_0
processor_sdk_rtos_am57xx_2_00_00_00
uia_2_00_03_43
xdais_7_24_00_04
xdctools_3_31_00_24_core
xdctools_3_31_01_33_core
xdctools_3_31_02_38_core
I have also installed any updates available.