This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

I2cLed Demo

Hi

 i2c_led example


I followed the instructions "Flashing Binaries to SPI Flash on ICE V1/V2 Using CCS" from the

"AM335x SYSBIOS Industrial SDK Getting Started Guide" pdf. Eresing the Flash works, but programming not.

I get the following outputs:

[CortxA8]
AM335x ISDK Flasher Version - 2.0.1 for ICEv2
SPI id selected - 0
Manufacturer ID read is 0xef.
Device ID read is 0x16.
Enter Operation [1 - Flash ] [2 - Erase] :
1
Enter the binary type [0-Bootloader, 1-Other ]
1
Enter the Offset in bytes (In HEX. eg:- bootloader :0x0 app : 0x20000)
20000
Load .bin file to 0x80100000 and Enter 0 to continue
0


It Doesnt go any further and is stuck at this point

Thanks 

Adnan

ICE AM 3359 v2 : 6 CCS / 6_42_03_35 SYSBIOS /3_32_00_06 XDCtools / 2_24_02_31 NDK