This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Automatic inlining in C6678 with CGTv7.4.2

Other Parts Discussed in Thread: SYSBIOS

Hi,

I have a c file from a speech codec that has fft functions. I am currently using O3 to build our project.

In order to qualify some loops, I had to inline some local functions (all functions in the same c file).
This helped and I got some loops qualified.

My understanding is that compiler does automatic inlining for O3 when all the function source code is visible. Then, why did I have to force it to inline?

I am working on C6678
XDC tools: version 3.25.05.94
SYSBIOS: version 6.33.06.50
CodeGenTools: version 7.4.2

--
Thanks!

Regards,
Sarvani Chadalapaka
HPC Systems Engineer
Signalogic Inc.