Other Parts Discussed in Thread: MSP430F47193, MSP430F47197, MSP430F47196
I just start to work on an energy meter project. I may use MSP430F47193.
I need some help to choose which IDE I should use, IAR or CCS4.x
I already have CCS4.x Platium. But
- Unlike IAR, I was told that CCS4 does not have 64bit long long int which may be a good thing to have for an energy meter;
- CCS4.x does support MSP430F47196 and MSP430F47197, but I did not find command file for MSP430F47193 in CCS4.x.
Is CCS4 the right compiler for an energy meter application using MSP430F47193? If it is, which command file should I use for 47193?
Thanks.
Chun