I am just starting to learn how to use CCS4 and have spent two hours or so reading many posts and guides from the wiki but can not find a simple explanation on how to approach multiple revisions of the same CCS4 project. I am new to Eclipse and CCS4 coming from CCSV3.1 so apologies for what seems like a trivial question?
To explain further:
I start with PROJECT1_VERSION1 in WORKSPACE1 and develop as required.
I now want to leave PROJECT1_VERSION1 as a baseline but continue development starting with a copy of PROJECT1_VERSION1.
What approach should I take to create PROJECT1_VERSION2 and where should it go (WORKSPACE1 or WORKSPACE2)?
I do not want to start off with a directory/workspace scheme that I will live to regret!
Regards, Andrew.
PS - assume a simple project - i.e. no linked files.