Other Parts Discussed in Thread: OMAP-L137
I'm trying to set up a Spectrum Digital OMAP-L137 EVM (possibly also referred to as the DA830?) with CCS v6. I've installed the latest SYS/BIOS and associated files. I can compile and load an example generic C674x project (benchmark).
However, when I attempt to start debugging I get an error that the license cannot be acquired and that it only supports XDS100 class or EVMs with onboard emulation. This board has an onboard XDS510 - is there an additional license I need? I have activated the SDK-OMAPL137-U part and Activation ID from the kit on my TI account but this dos not appear to generate any additional CCS license.