Hi there,
I have HPP files with some inline code. CCSv6 does not recompile them when they are changed. I know that this issue was present in CCSv5. Is it still the case for CCSv6?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
jown said:I clearly have this issue. The changes in the hpp file don't take effect until I recompile the project.
There is one known CCS issue that we are currently tracking:
"Making changes to a header file does not trigger rebuild of the source file that includes that header file".
The bug tracking # is SDSCM00051798 and it will be fixed in the next release of CCS scheduled for end of March.
I suspect you are hitting this same issue, so I would recommend giving 6.1.3 a try when it is released, or if you are able to post a small reproducible test case we can also check it when an internal build of the next version becomes available.