Other Parts Discussed in Thread: DRV8846, DRV8846EVM, INSTASPINUNIVERSALGUI
Did this ever get resolved? I am having a similar issue with the DRV8846_GUI. I can get to the point where I see the same image as JohnS with the "x's" on every icon,. After I connect my DRV8846EVM to my USB port the red x's remain, but my device shows up as the correct COM device number. I am seeing the blinking green "Status" LED on the dev board to indicate a USB connection.
I've installed the included FTDI driver using XP SP2 compatibility mode, and also tried the latest from FTDI (v2.12.00) using both compatibility mode as well as under Windows 7 mode. I am using GUI Composer Runtime CCS v6.1.1
-Joseph