Other Parts Discussed in Thread: CONTROLSUITE
I am using TI FM28335 MCU. I would like to know if there is any limitation of the compiler brought by CCS6. That is, do we need to buy a special compiler or software from TI in order to have unlimited feature? I am asking so because when I compile the program I edited, I found that if the length of the code is longer than a certain level, then the compiler just stopped there without any indication. If I remove some sentences in the code, then the compilation can be finished without problems.