Other Parts Discussed in Thread: CCSTUDIO
I am stuck in a 'loop' now of uninstalling CCS - reinstalling it, and having the installation fail.
It started when I tried to re-run the installer to add the spectrum digital drivers. I need the drivers for the XDS PROTRACE.
I hadn't installed CCS with SD drivers so I reran the installer. Then I got an error while "Installing com.sd.ccstudio.emulation.win32" was running.
A small window appears that says "An error has occurred during installation" but doesn't give any more information.
If I hit OK ccs will start but the spectrum digital emulators do not show up in the target configuration file editor.
I have also tried from this point 'check for updates' and 'uninstall feature' then 'install new software'.. various ways to get rid of and refresh that com.sd.ccstudio.emulation.win32. None work - all fail during the reinstall the same way as described above.
I've tried two different installation paths as well F:\ti and C:\ti .. no difference. Running out of ideas. Any thoughts?
(Also I can't find any *other* / standalone package to install the SD Drivers. SD's website seems to stop in time at about CCSv4.
And the PROTRACE emulator isn't even listed as a product - which concerns me a bit.)
This is a screen cap of it getting stuck again (new install)