I must import an old CCSv3.3 project in to the new CCSv6 or CCSv5.
I read the wiki and youtube and import it with the "Import Legacy CCSv3.3 Projects..."
Problems:
1. At the next step "Select Compiler" there are no results in the table. So there is nothing I could choose.
So I finished without choose an compiler.
2. The project was imported with an project.log:
!ERROR: Unknown device 'TMS320C24XX'!
When I try to create a new TargetConfiguration-File - Custom Configuration, there I can't choose the TMS320_24______
How can I get this CPU to the CCSv6?
Before that I downloaded and installed the ti_cgt_c2000_4.1.3_setup_win32.exe from http://software-dl.ti.com/codegen/non-esd/downloads/download.htm.
Thank you very much in advance