Other Parts Discussed in Thread: MSP-FET
During debug configuration getting following error.
Device Manage in Window 10 under Ports show "MSP Debug Interface (COM65) which matches. Beside, there is no option of configuring debug port# in code composer- where is COM65 coming from- is it hard coded?
MSP430: Can't Initialize Target CPU: **Error**: Serial Communication failed at port: COM65, baud rate:9600! To use serial monitor, please ensure the following prerequisites are satisfied: 1. Make sure the cable is plugged into both the target and the host on the right COM port. 2. Make sure a compatible target side serial monitor is loaded and running on the target device.