Other Parts Discussed in Thread: TMS570LS1224
Hi,
I'm have TI ARM Compiler v5.2.6 (linux version), target device is TMS570LS1224 and found problem on C++ templates and #pragma INTERRUPT(IRQ).
In next example #pragma INTERRUPT(IRQ) is ignored and no warning is issued. Static method interruptHandler() is compiled as *normal* method.
//header file
template <typename InterruptDriver>
class Foo {
template<std::size_t INT_CHANNEL>
static void interruptHandler();
}
#pragma INTERRUPT(IRQ)
template <typename InterruptDriver>
template<std::size_t INT_CHANNEL>
static void interruptHandler()
{
//some code
}
If merhod body is inlined into class (template) declaration like in next example, everything is OK. Method is compiled as IRQ handler.
//header file
template <typename InterruptDriver>
class Foo {
#pragma INTERRUPT(IRQ)
template<std::size_t INT_CHANNEL>
static void interruptHandler() {
//some code
}
}
I belive, that first example should work too, or am I wrong?
Thanks
Libor Votocek*